Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design DMA Kernel panics
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Subscribers 363 subscribers
  • Views 2547 views
  • Users 0 members are here
Related

DMA Kernel panics

e14 Contributor
e14 Contributor over 9 years ago

Hi,

over the past few days, I desperately tried to build my own bootloader kernel etc. without using Petalinux, because I already have my own ecosystem based on Yocto and meta-xilinx.

I started with all git HEADs for U-Boot, ATF and the Linux kernel and wanted to use U-Boot as an SPL. Which didn't work at all, because the newest git HEAD of U-Boot actually needs a PMU firmware in version 0.3 which is nowhere to be found. That's very annoying!

So I fell back to older releases of all the components which were 2016.4. I managed to get a fully working FSBL, U-Boot 2016.4 with ATF and Linux 2016.4. When including the PMU firmware in the boot image, the 4.6 kernel breaks because the SD-Card controller fails to initialize. It works without loading a custom PMU firmware. I can't use the current 4.9 kernel, because this in turn needs a PMU firmware with version 0.3. AAAHHH!

Okay, back to kernel 4.6 without a PMU firmware then. It booted up into my userland and I was quite happy. But after a while of using the system on this kernel, I get a bunch of kernel panics caused from different DMA operations happening in different components. Sometimes the SD-Card fails, sometimes the MACB NIC driver. Even the slightest bit of load on the network card causes a fatal kernel panic in the interrupt context.

Then I tried Petalinux 2016.4. I can't get this to work properly either. First the U-Boot complained about a messed up memory config in the device tree (https://www.xilinx.com/support/answers/68390.html) which I eventually managed to fix by editing the correct dts file which doesn't get overwritten by the generation tools. But then I can't properly boot the system, because the U-Boot confuses the first SHDC controller with the second one. Even though I boot from the external card, it always wants to load the kernel from the eMMC.

I basically gave up for now. Is there *any* combination of compoenents that work at all on this chip and which do not immediately crash?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 9 years ago in reply to tchoyt +1
    I have a patch for u-boot-xlnx and linux-xlnx which adds device trees and other support for the Ultrazed on an IOCC. I reenabled a bunch of peripherals like the eMMC, QSPI and I2C1 in your FPGA image to…
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Yes, I found this afterwards, but it's basically what I did on my own as well.

    According to their known issues, they face the same problem:

    There seems to be a significant issue with the DMA and/or Interrupt controller. Any sustained reads or writes will result in a kernel panic associated with either an interrupt controller timeout or a DMA failure; even when running the simple LED counting test above. This could be the result of the current MACB driver’s interrupts being implemented with polling but it’s not limited just to reads/writes over the network. Failures occur while reading and writing from a USB2 device as well as local copies on the SD card.

    I even have kernel development experience du to all the stuff I did with the original Zynqs, but I don't even know where to start debugging is in the drivers. I also backported the 4.9 MACB driver to my 4.6 kernel, but the issues still exist. So either the memory corruption caused by this driver isn't fixed or it's a bigger problem in another component.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Yes, I found this afterwards, but it's basically what I did on my own as well.

    According to their known issues, they face the same problem:

    There seems to be a significant issue with the DMA and/or Interrupt controller. Any sustained reads or writes will result in a kernel panic associated with either an interrupt controller timeout or a DMA failure; even when running the simple LED counting test above. This could be the result of the current MACB driver’s interrupts being implemented with polling but it’s not limited just to reads/writes over the network. Failures occur while reading and writing from a USB2 device as well as local copies on the SD card.

    I even have kernel development experience du to all the stuff I did with the original Zynqs, but I don't even know where to start debugging is in the drivers. I also backported the 4.9 MACB driver to my 4.6 kernel, but the issues still exist. So either the memory corruption caused by this driver isn't fixed or it's a bigger problem in another component.