Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design DMA Kernel panics
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Subscribers 363 subscribers
  • Views 2547 views
  • Users 0 members are here
Related

DMA Kernel panics

e14 Contributor
e14 Contributor over 9 years ago

Hi,

over the past few days, I desperately tried to build my own bootloader kernel etc. without using Petalinux, because I already have my own ecosystem based on Yocto and meta-xilinx.

I started with all git HEADs for U-Boot, ATF and the Linux kernel and wanted to use U-Boot as an SPL. Which didn't work at all, because the newest git HEAD of U-Boot actually needs a PMU firmware in version 0.3 which is nowhere to be found. That's very annoying!

So I fell back to older releases of all the components which were 2016.4. I managed to get a fully working FSBL, U-Boot 2016.4 with ATF and Linux 2016.4. When including the PMU firmware in the boot image, the 4.6 kernel breaks because the SD-Card controller fails to initialize. It works without loading a custom PMU firmware. I can't use the current 4.9 kernel, because this in turn needs a PMU firmware with version 0.3. AAAHHH!

Okay, back to kernel 4.6 without a PMU firmware then. It booted up into my userland and I was quite happy. But after a while of using the system on this kernel, I get a bunch of kernel panics caused from different DMA operations happening in different components. Sometimes the SD-Card fails, sometimes the MACB NIC driver. Even the slightest bit of load on the network card causes a fatal kernel panic in the interrupt context.

Then I tried Petalinux 2016.4. I can't get this to work properly either. First the U-Boot complained about a messed up memory config in the device tree (https://www.xilinx.com/support/answers/68390.html) which I eventually managed to fix by editing the correct dts file which doesn't get overwritten by the generation tools. But then I can't properly boot the system, because the U-Boot confuses the first SHDC controller with the second one. Even though I boot from the external card, it always wants to load the kernel from the eMMC.

I basically gave up for now. Is there *any* combination of compoenents that work at all on this chip and which do not immediately crash?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 9 years ago in reply to tchoyt +1
    I have a patch for u-boot-xlnx and linux-xlnx which adds device trees and other support for the Ultrazed on an IOCC. I reenabled a bunch of peripherals like the eMMC, QSPI and I2C1 in your FPGA image to…
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Okay, this is really getting frustrating now. The just released Vivado 2017.1 contained the PMU firmware 0.3 which enables me to use a current u-boot and kernel.

    I built a current u-boot (git HEAD on master) after adding a simple board config and the device tree for the Ultrazed. I then build the current kernel (git HEAD on master) after adding the device-tree as well. So far it's always booting and then it randomly crashes after a few seconds in the userland. Here are only three panics that I encountered:

    https://www.zerobin.net/?059d2ba739accd93#ghawrpPklL+rgKzjx+6SPuP82mpMqm9q/wKfWHtyDlU=
    https://www.zerobin.net/?03616b0a1d07b1df#D3Gv2nQiN7eFtG9DHAkv8BzZ+ztfVbDICO0orU034T4=
    https://www.zerobin.net/?99808a36612168c1#xGMCeCP/JlcQ/1FznPS+HpgoTU0VoONWwpc71hMDhqs=

    Wat.

    Any ideas? This almost smells like broken hardware. It's just way too random.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Okay, this is really getting frustrating now. The just released Vivado 2017.1 contained the PMU firmware 0.3 which enables me to use a current u-boot and kernel.

    I built a current u-boot (git HEAD on master) after adding a simple board config and the device tree for the Ultrazed. I then build the current kernel (git HEAD on master) after adding the device-tree as well. So far it's always booting and then it randomly crashes after a few seconds in the userland. Here are only three panics that I encountered:

    https://www.zerobin.net/?059d2ba739accd93#ghawrpPklL+rgKzjx+6SPuP82mpMqm9q/wKfWHtyDlU=
    https://www.zerobin.net/?03616b0a1d07b1df#D3Gv2nQiN7eFtG9DHAkv8BzZ+ztfVbDICO0orU034T4=
    https://www.zerobin.net/?99808a36612168c1#xGMCeCP/JlcQ/1FznPS+HpgoTU0VoONWwpc71hMDhqs=

    Wat.

    Any ideas? This almost smells like broken hardware. It's just way too random.