Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZed IOCC Ethernet Not Functioning
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 431 views
  • Users 0 members are here
Related

UltraZed IOCC Ethernet Not Functioning

e14 Contributor
e14 Contributor over 9 years ago

I am unable to connect to a network via the Ethernet on the IOCC. The following are the various attempts at connecting:

 

UltraZed OOBE Linux (DHCP - Default OOBE Settings)

  1.   Connected the UltraZed to the network with DHCP
  2.   Never obtains an ip address.

UltraZed OOBE Linux (Static IP)

  1.   ifconfig eth0 192.168.1.216 netmask 255.255.255.0 broadcast 192.168.1.255
  2.   ping -c 4 192.168.1.1  # Ping Gateway
  3.   No Response

Xilinx LwIP Echo Server Example

  1.   Unable to connect / No Response

Network Cables test good & multiple tried.

 

Could there be a potential hardware issue with the network interface?

 

Thanks,

Ryan

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    I overlooked an Answer Record regarding this: https://www.xilinx.com/support/answers/66553.html 

    It seems only 1G/Full is currently supported and I was using a 100M Switch. Connecting to a gigabit switch did the trick.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer