Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Questions for FMC-MULTI-CAM4
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Subscribers 362 subscribers
  • Views 3182 views
  • Users 0 members are here
Related

Questions for FMC-MULTI-CAM4

prornetheus
prornetheus over 7 years ago

Hello,

 

I want to use FMC-MULTI-CAM4 for camera input to my system.

 

But there is no Vivado project for RTL, and modified project which extracted from SDx project does not working (it seems it could not initialize cam module)

and DisplayPort does not working in reference design (prebuilt)

 

Could you give me Vivado 2018.2 project for FMC-MULTI-CAM4 ?

 

I just need Single channel of GMSL camera

but if it does not working, 4-ch GMSL project for vivado is ok for me.

 

My systemreVISION Tutorial (Prebuilt)reVISION Tutorial (re-built)
Project typeRTL, VivadoHLS, SDx

Vivado

(SDx -> Extract synth project from "workspace\filter2d_optflow\Release\_sds\p0\vivado\prj" -> remove HDMI at Vivado and rebuilt)

CameraUVCGMSL -> CSI-2GMSL -> CSI-2 (Sensor not detected)
DisplayDP onlyHDMI / DP, but DP not workingDP only, but DP not working
TestsUVC to DP : Working

GMSL to HDMI : Working

GMSL to DP : Not working

UVC to HDMI : Working

UVC to DP : Not working

GMSL to HDMI : Not working

GMSL to DP : Not working

UVC to HDMI : Not working

UVC to DP : Not working

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 7 years ago

    Hi,

     

    What board are you looking to connect the camera to?

     

    Thanks,

    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • prornetheus
    0 prornetheus over 7 years ago in reply to jafoste4

    I'm using ZCU102 for cameras.

     

    Thanks, Hanseung.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • albertabeef
    0 albertabeef over 7 years ago in reply to prornetheus

    Hello,

     

    Please use the lastest 2018.3 version of the revision platform for ZCU102.

       http://ultrazed.org/sites/default/files/design/FMC_MULTICAM4_REVISION_Tutorial_2018_3_01.zip

     

    This platform contains the hardware design in DSA format (design source archive).  You can open the hardware design by typing the "open_dsa" command in the TCL console.

     

    This platform also has a pre-built image that works with 1 camera and the DisplayPort output, located in the sdcard directory.

     

    Note that the single camera configuration can be configured in the device tree when building petalinux images.

     

    Hope this helps !

     

    Mario

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • prornetheus
    0 prornetheus over 7 years ago in reply to albertabeef

    Thanks Mario

     

    GMSL(4ch, 1ch at device tree) to DP works well with 2018.3 project from your link.

     

    but when I try to remove HDMI tx/rx and three other GMSL pipeline, Sensor not initialized.

     

    [   12.415188] AR0231 24-0011: Enter
    [   12.418507] AR0231 24-0011: id 0 name ar0231
    [   12.422826] AR0231 24-0011: AR0231 probe Success Done
    [   12.427978] AR0231 24-0010: Enter
    [   12.431292] AR0231 24-0010: id 1 name ar0231-i2c
    [   12.435931] AR0231 24-0010: AR0231 probe Success Done
    
    ...
    
    
    root@xilinx:/media/card# ./video_cmd -S
    [vcap_gmsl] vcap_gmsl_init ...
    [vcap_gmsl] csi_set_act_lanes ...
    [vcap_gmsl] v4l2_csi_set_ctrl ...
    [vcap_gmsl] V4L2_CID_TEST_PATTERN ... 0
    [vcap_gmsl] SET_CTRL : ID=0x009F0903, VALUE=0x00000000 ...
    ERROR(../src/mediactl_helper.c:100) : Entity 'AR0231.25-0011' not found
    Aborted

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • albertabeef
    0 albertabeef over 7 years ago in reply to prornetheus

    Hanseung,

     

    Notice that there is a hard-coded I2C bus/device in the mediactl_helper.c source file:

         ERROR(../src/mediactl_helper.c:100) : Entity 'AR0231.25-0011' not found

     

    When you remove I2C devices from the device tree content, these ids will change.

    In the case of your modified design, the new id appears previously in the boot log you provided:

         AR0231 24-0010

     

    You will need to change the application code to reflect this change.

     

    The code you are looking for is located in the petalinux recipe for the xlnxvideosrc plug-in.

         project-spec/meta-user/recipes-apps/gst-plugins-xlnx/files/gst-plugins-xlnx.zip

     

    It will also be located in the petalinux recipe for the video_qt2 application.

         project-spec/meta-user/recipes-apps/video-qt2files/video-qt2.zip

     

    For additional help on how to rebuild these components individually (for testing), please refer to the following Xilinx wiki page:

         https://xilinx-wiki.atlassian.net/wiki/spaces/A/pages/46923869/Zynq+UltraScale+MPSoC+Base+TRD+2018.3+-+Design+Module+5

     

    Regards,

     

    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • prornetheus
    0 prornetheus over 7 years ago in reply to albertabeef

    Thank you mario. Problem solved.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rifat0231
    0 rifat0231 over 4 years ago in reply to albertabeef

    The link for the 2018.3 version of the revision platform for ZCU102 redirects to some other pages. Can you please share these files with a valid link?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Foysal
    0 Foysal over 4 years ago in reply to prornetheus

    Hello, this thread was helpful. However, the link for the ''FMC_MULTICAM4_REVISION_Tutorial_2018_3_01.zip" file is not working. Can anyone please share me the updated link or share me the files in any medium. Thanks a lot in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tcao
    0 tcao over 2 years ago in reply to albertabeef

      Hi Mario and others, I'm interested at doing a project based on FMC-MULTICAM4, do you still have valid download urls for followings? 

    FMC_MULTICAM4_REVISION_Tutorial_2018_3_01.zip and

    Hardware User Guide
    www.element14.com/.../avnet-multi-camera-fmc-module-hug-1v02pdf

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • albertabeef
    0 albertabeef over 2 years ago in reply to tcao

    That product is now obsolete, so there is no new development being made for it.

    The latest designs from Avnet for UltraZed-EV (only) can be found on Hackster.io:

    • https://www.hackster.io/AlbertaBeef/quad-face-detection-with-the-ultrazed-ev-and-multi-cam-fmc-0fbc33
    • https://www.hackster.io/AlbertaBeef/automatic-activation-of-a-simple-white-balance-algorithm-7d1cb8

    The latest designs from Xilinx for ZCU106 (only) can be found on AMD/Xilinx's wiki:

    • https://xilinx-wiki.atlassian.net/wiki/spaces/A/pages/2077524005/Zynq+UltraScale+MPSoC+ZCU106+VCU+Multi-Stream+ROI+TRD+using+Avnet+Quad+Sensor+2021.1

    If you search on AMD/Xilinx's wiki pages, you may find versions of the demo for other ZCU10x carriers.

    Hope this helps !

    Mario.