Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design USB3 devices detected as USB2 in petalinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 1238 views
  • Users 0 members are here
  • ultrazed-ev
  • usb3.0
  • petalinux
Related

USB3 devices detected as USB2 in petalinux

jlesquer
jlesquer over 7 years ago

Hello,

 

I'm trying to connect a USB3 camera to the Ultrazed-EV starter kit using petalinux, and I can see that the camera is being detected but as a USB2 device, here is the shell log:

image

 

I set up the USB mode jumpers in the board as a default HOST mode indicated here: http://zedboard.org/sites/default/files/documentations/UZ-EV-CC-UG-ver1.pdf (page 12), also tried OTG configuration with same results.

 

In order to connect the camera to the board I'm using the next adapter:

https://www.kenable.co.uk/en/usb-cables-adapters/usb-30-superspeed/7005-kenable-usb-30-superspeed-a-female-to-micro-b-male-10-pin-adapter-007005-5055383470051.html?gclid=EAIaIQobChMI4PmPkMKO4gIVmIjVCh1dxAukEAQYASABEgJzBvD_BwE

 

The camera is detected and works as USB3 device with not problems in a windows or linux PC (without the above USB adapter).

I tried another devices as a USB3.0 memory stick and they are also detected as USB 2.0 device....

 

Any ideas what could it be the problem?

 

Thanks in advance.

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 7 years ago

    Hi there,

     

    While I'm looking into the configuration we used to test this, can you confirm that you set 3 jumpers to host mode?

     

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jlesquer
    0 jlesquer over 7 years ago in reply to drozwood90

    Hi,

     

    Thanks for the reply.

    Yes, I've got the next jumper setup:

    JP12      ON

    JP21      pin 2-3

    JP23      pin 1-2

     

    I looked around the web and I've found some clues that it could be related to the USB3 adapter....

     

    I'm trying a few different adapters and none are working so far still detecting the USB3 devices as USB2.

     

    I've got a couple of questions:

    1) Did you test USB3 interface successfully with an adpater with this boards? if so, could you please point me to a working one?

     

    2) On the other hand I opened the provided 2018.2 BSP Vivado HW design and  in the zynqMP processor settings the USB3 VBUS is not selected, do I need to activate this option?

     

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jlesquer
    0 jlesquer over 7 years ago in reply to drozwood90

    Hi,

     

    Thanks for the reply.

    Yes, I've got the next jumper setup:

    JP12      ON

    JP21      pin 2-3

    JP23      pin 1-2

     

    I looked around the web and I've found some clues that it could be related to the USB3 adapter....

     

    I'm trying a few different adapters and none are working so far still detecting the USB3 devices as USB2.

     

    I've got a couple of questions:

    1) Did you test USB3 interface successfully with an adpater with this boards? if so, could you please point me to a working one?

     

    2) On the other hand I opened the provided 2018.2 BSP Vivado HW design and  in the zynqMP processor settings the USB3 VBUS is not selected, do I need to activate this option?

     

    Thanks.