Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZed Board Support Package
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 360 subscribers
  • Views 929 views
  • Users 0 members are here
Related

UltraZed Board Support Package

bhoevding
bhoevding over 7 years ago

Hello,

 

does anyone know when the Avnet-UltraZed-BSP-2018.3 or Avnet-UltraZed-BSP-2019.1 will be released?

 

I am uncertain about using PetaLinux Tools V2018.3 without the Avnet BSP.

Which contents are in the Avnet-BSP and what is the difference between generating a custom BSP from Vivado -> PetaLinux Tools and using the one from Avnet?

 

Please let me know about your recommendation.

 

best regards,

 

Bjørn

 

UltraZed-EG Embedded Linux Using Xilinx Tools Forum UltraZed

  • Sign in to reply
  • Cancel
  • 100padudle
    0 100padudle over 7 years ago

    Hello Bjørn,

     

    Did you ever get a response to this?

     

    The last BSP for the Ultrazed I see is 2018.2.  To run Petalinux 2018.2 I will have to setup a special virtual machine to run Ubuntu 2016.04 LTS. I would rather not go to all that trouble.  I would much rather have a 2019.1 BSP for the board.

     

        Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bhoevding
    0 bhoevding over 7 years ago in reply to 100padudle

    Hello Peter,

     

    no, unfortunately I didn't get any answers.

     

    For my applications I am currently using the Xilinx-v2019.1-Toolchain (Vivado, SDK, PetaLinux Tools) and it seems to work.

    The BSP is just a reference design, which is not essentially required for development.

     

    You can generate all the required Boot-Files, Device Tree and Kernel Image using the current Xilinx Toolchain.

    For more information I recommend the UG1144 PetaLinux Tools Manual (P. 21) which explains in depth, how to generate the required Embedded Linux Components.

    The BSP will then be generated through your Vivado-Hardware-Design.

     

    image Make sure to use one of the recommended OS Distributions from UG1144 (P. 9), since the Yocto Release in PetaLinux Tools is only compatible to some Releases. (Debian 9 works as well)

     

    An Example to get started with the UltraZed-EG-IOCC:

    petalinux-create --type project --template zynqmp --name <PROJECT_NAME>

    let me know if you need anything else and best of luck.

    Bjørn