Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZed Ethernet MAC ID
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 3 answers
  • Subscribers 361 subscribers
  • Views 2059 views
  • Users 0 members are here
Related

UltraZed Ethernet MAC ID

jdehaven
jdehaven over 7 years ago

The UltraZed EG SOM documentation has the following note about the Ethernet MAC ID:

image

However, page 5 of the IO carrier card schematic shows the MAC ID - EEPROM, but does not explain how the ID is implemented.

image

 

Does the UltraZed SOM come with a unique MAC ID that can be used by the customer, or does the customer carrier card need to supply a unique MAC ID to the UltraZed SOM?

 

Thanks,

John

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 6 years ago

    Hi John,

     

    I also wrote a blog article that touches on this topic:

     

    Homestretch To Production - MAC Address Programming Approaches

     

    My article also proposes an alternative to the U-Boot MAC ID programming method clem57 pointed out above.  The method I used boots the system with the default MAC ID, but then reassigned the network interface to the MAC ID read off the EEPROM.  Here is the script that I used on UltraZed-EG to read from the MAC ID EEPROM:

     

    https://github.com/Avnet/petalinux/blob/master/configs/meta-user/uz3eg_iocc/recipes-apps/mac-eeprom-config/files/mac_eep…

     

    The only other way I have seen this done elsewhere for systems booting from SPI Flash is to parse the QSPI Flash partition for U-Boot and overwrite the ethaddr environment variable so that the next time the system boots, U-Boot has already loaded the unique MAC address which is now also stored in NVM.

     

    Best Regards,

     

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 6 years ago

    Hi John,

     

    I also wrote a blog article that touches on this topic:

     

    Homestretch To Production - MAC Address Programming Approaches

     

    My article also proposes an alternative to the U-Boot MAC ID programming method clem57 pointed out above.  The method I used boots the system with the default MAC ID, but then reassigned the network interface to the MAC ID read off the EEPROM.  Here is the script that I used on UltraZed-EG to read from the MAC ID EEPROM:

     

    https://github.com/Avnet/petalinux/blob/master/configs/meta-user/uz3eg_iocc/recipes-apps/mac-eeprom-config/files/mac_eep…

     

    The only other way I have seen this done elsewhere for systems booting from SPI Flash is to parse the QSPI Flash partition for U-Boot and overwrite the ethaddr environment variable so that the next time the system boots, U-Boot has already loaded the unique MAC address which is now also stored in NVM.

     

    Best Regards,

     

    -Kevin