Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZed-EV starter kit kernel boot problem.
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 1101 views
  • Users 0 members are here
Related

UltraZed-EV starter kit kernel boot problem.

dpechkin
dpechkin over 6 years ago

Hello!

 

I have the UltraZed-EV System-on-Module Starter Kit.

I have the petalinux-2019.1 and UltraZed-EV Carrier Card—PetaLinux 2019.1 Enhanced BSP.

 

I created a project and checked that the root file system type is initramfs.

And It was built successfully after these steps.

 

I set a switch to jtag mode (On-On-On-On) and upload u-boot via command: petalinux-boot --jtab --u-boot.

 

I set the server IP of the TFTP server and executed the command "run netboot" in the u-boot console.

The image is uploaded, and the kernel was started.

 

The kernel was hanged on after these lines:

console [ttyPS0] enabled at MMIO 0xff000000 (irq = 46, base_baud = 6249999) is a xuartps

[    3.535829] console [ttyPS0] enabled

[    3.539420] bootconsole [cdns0] disabled

[    3.539420] bootconsole [cdns0] disabled

[    3.547328] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 47, base_baud = 6249999) is a xuartps

 

The full console log is attached.

 

I have the same issue for the project for the SD card.

The switch was set to OFF-ON-OFF-ON for that rootfs type.

 

Maybe I missed some steps?

Anyone can give some advice?

Thanks in advance.

Attachments:
fulllog.txt.zip
  • Sign in to reply
  • Cancel
Parents
  • narrucmot
    0 narrucmot over 6 years ago

    Hi Dmitriy,

     

    The boot error you describe is what happens when the bitstream is not included as part of the boot process.  The PetaLinux boot command you want is:
    $ petalinux-boot --jtag --fpga --bitstream images/linux/system.bit --u-boot --verbose

     

    The '--verbose' is not required, but is often helpful.

     

    Likewise, to create a boot.bin that is suitable for SD card boot and that includes the PL bitstream, the PetaLinux package command is:

    $ petalinux-package --boot --fsbl images/linux/zynqmp_fsbl.elf --fpga images/linux/system.bit --uboot --force

     

    Attached is the boot log from a successful JTAG/TFTP boot you can use to validate your boot success.

     

    Cheers,

    Tom

     

    PS - Make sure to mark this question as answered if my reply has answered your question.  Thanks!

    Attachments:
    uz7ev_2019p1_bsp_jtag_bootlog.txt.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • narrucmot
    0 narrucmot over 6 years ago

    Hi Dmitriy,

     

    The boot error you describe is what happens when the bitstream is not included as part of the boot process.  The PetaLinux boot command you want is:
    $ petalinux-boot --jtag --fpga --bitstream images/linux/system.bit --u-boot --verbose

     

    The '--verbose' is not required, but is often helpful.

     

    Likewise, to create a boot.bin that is suitable for SD card boot and that includes the PL bitstream, the PetaLinux package command is:

    $ petalinux-package --boot --fsbl images/linux/zynqmp_fsbl.elf --fpga images/linux/system.bit --uboot --force

     

    Attached is the boot log from a successful JTAG/TFTP boot you can use to validate your boot success.

     

    Cheers,

    Tom

     

    PS - Make sure to mark this question as answered if my reply has answered your question.  Thanks!

    Attachments:
    uz7ev_2019p1_bsp_jtag_bootlog.txt.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • dpechkin
    0 dpechkin over 6 years ago in reply to narrucmot

    Hi Tom,

     

    I tested boot via TFTP using your command. It works.

     

    Thanks.