Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Ultra96 Anyone tried to use the HS Connector with 1.8V logic
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 358 subscribers
  • Views 923 views
  • Users 0 members are here
Related

Ultra96 Anyone tried to use the HS Connector with 1.8V logic

100charlesb
100charlesb over 6 years ago

I am aware that the HS connector uses 1.2V logic but is there a way to bodge it to operate with 1.8V logic?

I notice the VCCO_HP rail is powered by a TPS6508641 (LDO03A) which can be programmed to 1.5 volt

then looking at Xilinx DS925 it seems that at VCCO + 0.3V the HP bank can operate at 100% of UI (unit interval).

I suspect it would not be possible to cut the track and insert 1.8V as it is a multi-layer board.

 

I made a little adapter board that connects the Ultra96 to a high speed ADC but had assumed it was all 1.8v

logic so I am scuppered if I can't find a work around.

 

 

- Charles

  • Sign in to reply
  • Cancel

Top Replies

  • bhfletcher
    bhfletcher over 6 years ago +1 suggested
    For both Ultra96-V1 and Ultra96-V2, the HS Connector has a total of 34 PL IOs as follows: 2 from Bank 26 with VCCO = 1.8V -- I assume this is not enough for what you need 32 from Bank 65/66 with VCCO …
  • bhfletcher
    0 bhfletcher over 6 years ago

    For both Ultra96-V1 and Ultra96-V2, the HS Connector has a total of 34 PL IOs as follows:

    • 2 from Bank 26 with VCCO = 1.8V -- I assume this is not enough for what you need
    • 32 from Bank 65/66 with VCCO = 1.2V

     

    I think what you propose may work with the Ultra96-V1. Please let us know if reprogramming the TPS6508641 to 1.5V worked.

     

    For those who have the same question with Ultra96-V2, I will add a bit more analysis. The Ultra96-V2 has a bit more flexibility given the Infineon PMICs allow more programmable voltage range, but a design decision to combine the 1.2V HP Bank rail and the 1.2V USB Hub rail complicates things.

     

    Looking at the Bank 65/66 VCCO specifically for Ultra96-V2:

    • VCCO_65 is tied to net +VCCO_HP
    • VCCO_66 is tied internally to VCCO_65, so also +VCCO_HP
    • +VCCO_HP is Channel B output of U11, PMIC IRPS5401, Addres = 0x13
    • +VCCO_HP is programmed to operate at 1.2V and 2.0A
    • Besides VCCO_65, what else is connected to +VCCO_HP?
      • Pull-up for FAN_PWM control, which is also on Bank 65
      • VDD12 on U16, Microchip USB5744 USB Controller Hub
        • VDD12 Abs Max = 1.32V

     

    Since the PMIC is a programmable device, you could use the Infineon tools and Dongle to reprogram 0x13 Channel B output voltage to 1.8V. However, that exceeds the USB5744 absolute max on VDD12. If you didn't care about the USB functionality on Ultra96-V2 and you had the means, you could remove the USB5744 and then reprogram U11 to do what you want.

     

    It might be easier to switch to something that is a lot more versatile like the UltraZed-EG platform.

     

    Bryan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer