Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design lwip autonegotiation fails when using FSBL
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 360 subscribers
  • Views 3261 views
  • Users 0 members are here
  • ultrazed
Related

lwip autonegotiation fails when using FSBL

dat63
dat63 over 6 years ago

Hi,

I have a Vivado design based on UltraZed-EV SOM. I am using Vitis 2019.2 to develop an application that makes use of a lwip TCP server. It happens that if I launch the application by selecting the psu_init.tcl file option in the Target Setup Configuration of the debugger everything works fine. If I select the initialization through the FSBL file, the lwip autonegotiation procedure always fails with the following messages:

Auto negotiation error
Phy setup error
Phy setup failure init_emacps
Ethernet link down

Needless to say that in the final application I need to use the FSBL

Any help is very much appreciated

Daniele

  • Sign in to reply
  • Cancel
  • drozwood90
    0 drozwood90 over 6 years ago

    Hi there,

     

    I'd have to confirm with the SW group, but as far as I know, the networking "stuff" is all initialized and re-initialized between those two steps. This means hardware, clocks, and other control loops.

    That is probably the issue you are seeing.  I'll pass this along to see if I can get some kind of confirmation.

     

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • narrucmot
    0 narrucmot over 6 years ago

    You may want to take a look at Xilinx XAPP1026 -  lwIP Application Examples and XAPP1306 - PS and PL-Based Ethernet Performance with lwIP Stack.  I believe the prescribed method is to use the psu_init.tcl to init the Zynq PS when launching the lwIP app, etc. via the Xilinx SDK, and use the FSBL when booting the lwIP apps via SD card.

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dat63
    0 dat63 over 6 years ago in reply to narrucmot

    Hi Tom,

    what you suggest is exactly what I am doing; I am using the lwIP TCP server demo application (no custom code) and it simply does not work when I use the FSBL either from the debugger or booting from the SD card

    Daniele

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • enelson_ngrf
    0 enelson_ngrf over 5 years ago in reply to dat63

    Hello Daniele,

     

    Did you resolve this?  I am having the exact same problem.

     

    Thanks!

    Elliott