Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design petalinux 2019.1 build error with ultrazed EV 2019.1 bsp
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 2 answers
  • Subscribers 359 subscribers
  • Views 985 views
  • Users 0 members are here
  • petalinux board support packages
  • ultrazed-ev carrier card
Related

petalinux 2019.1 build error with ultrazed EV 2019.1 bsp

jkmenon-ign
jkmenon-ign over 6 years ago

Hi

 

I am using the Xilinx petalinux tool version 2019.1 to build the images for booting up the Ultrazed EV starter Kit.

I have downloadedUltraZed-EV Carrier Card—PetaLinux 2019.1 Enhanced BSP file from the reference-designs in https://www.element14.com/community/community/designcenter/zedboardcommunity/ultrazed/ultrazed-ev

I have a sample HDF exported from Vivado 2019.1 also.

 

Here are the steps that i followed ( method 1)

1. petalinux-create -t project -s <path-to-BSP/uz7ev_evcc_2019_1.bsp>

2. petalinux-config --get-hw-description=<path-to-HDF>

3. petalinux-build

 

When I used the template option without giving BSP and only specifying the HDF, the build was successful. Reference to this link (https://www.avnet.com/wps/portal/us/resources/article/building-petalinux-for-the-ultrazed-and-pcie-carrier-card/ )

step 1 replaced with "petalinux-create --type project --template zynqMP --name <project name> "

 

(method 2)

1. petalinux-create --type project --template zyncMP --name <project name>

2. petalinux-config --get-hw-description=<path-to-HDF>

3. petalinux-build

 

with method 2 the build was successful.

 

So If we are building without BSP, I found that the device tree binding will have missing device/nodes missing eth/usb peripherals and we have to add some of the peripherals manually.

 

My build environment is Ubuntu 16.04, with sufficient memory requirements.

 

What can be the possible solutions to build with BSP file and followed by configuration with HDF, is there anything I am missing out?

 

Thanks

Attachments:
petalinux_build_error.txt.zip
  • Sign in to reply
  • Cancel

Top Replies

  • narrucmot
    narrucmot over 6 years ago +1 suggested
    It appears as though there is some sort of mismatch between your custom HDF and the BSP. If you want to use a custom Vivado hw platform with this BSP, you may want to start with the known-good 'UZ7EV_EVCC…
  • narrucmot
    0 narrucmot over 6 years ago

    It appears as though there is some sort of mismatch between your custom HDF and the BSP.  If you want to use a custom Vivado hw platform with this BSP, you may want to start with the known-good 'UZ7EV_EVCC.xpr' Vivado project in the <>/hardware/UZ7EV_EVCC_2019_1 folder of the BSP.  This is the hw platform the BSP was built from, and can be used as the foundation for any customization you want to do.  Just make your changes, re-implement the design, export a new UZ7EV_EVCC.dsa file (be sure to include the bitstream), import that into the PetaLinux project with 'petalinux-config --get-hw-description=<path-to-DSA>', and do a new 'petalinux-build'.

     

    --Tom

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jkmenon-ign
    0 jkmenon-ign over 6 years ago in reply to narrucmot

    Hi Tom Curran,

     

    Thanks for the response, As you have mentioned we had some mistake/(missing port information) in the HDF which leads to the build issue, reinspecting the hdf in detail helped to solve the problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer