Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Vivado Hardware manager does not detect any devices on the UltraZed-EG SOM board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 4629 views
  • Users 0 members are here
Related

Vivado Hardware manager does not detect any devices on the UltraZed-EG SOM board

eran99
eran99 over 6 years ago

I'm connected to the Avnet UltraZed-EG SOM board using DLC10 USB-JTAG

adopter.
when I click on open-target and then auto-connect, the DLC10 is detected, and the UltraZed-EG is detected - I know that since it says:

Xilinx_tcf/Xilinx/00001877ae8201(0) "open", but if I unplug the jtag connector is says "closed".

However, it says Device Count 0 under properties, and I'm getting a message " No devices detected on target"

 

I set all 4 DIP switches to ON, which is 0000 for JTAG boot mode.

 

Is there any other setting or jumpers I need to deal with on the UltraZed board, or perhaps it's a driver issue?

 

Eran

  • Sign in to reply
  • Cancel
Parents
  • narrucmot
    0 narrucmot over 6 years ago

    Hi Eran,

     

    I suspect this may be a host OS or driver issue.

     

    Are you using a custom carrier card for the UZ3EG SOM, or the Avnet I/O or PCIe carrier card?  If using either Avnet carrier, you can use the SMT2 JTAG module instead.  I rarely use my Xilinx DLC10 JTAG pod any more, and when I do I often have trouble getting my host OS (Win10) and/or Ubuntu VM to recognize it.  I don't have the same trouble with the SMT2 JTAG module.  The SMT2 JTAG is also faster, so that is another benefit.

     

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • narrucmot
    0 narrucmot over 6 years ago

    Hi Eran,

     

    I suspect this may be a host OS or driver issue.

     

    Are you using a custom carrier card for the UZ3EG SOM, or the Avnet I/O or PCIe carrier card?  If using either Avnet carrier, you can use the SMT2 JTAG module instead.  I rarely use my Xilinx DLC10 JTAG pod any more, and when I do I often have trouble getting my host OS (Win10) and/or Ubuntu VM to recognize it.  I don't have the same trouble with the SMT2 JTAG module.  The SMT2 JTAG is also faster, so that is another benefit.

     

    --Tom