Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design No output in Serial/ttyUSB0
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 1870 views
  • Users 0 members are here
  • ultrazed
Related

No output in Serial/ttyUSB0

kumakichi
kumakichi over 4 years ago

Hi there,

 

We are working on a project on Ultrazed-ev board. (porting design from zcu106 to Ultrazed-ev).

The out of box firmware works fine.

But when booting with the one built from the xsa we desgined, there is nothing shown in the uart/serial port.

 

Information:

baudrate configured to be 115200-8-N-1.

#booting from SD card

--SD card folders:

partition1: fat32

boot

|-- BOOT.BIN

|-- boot.scr

`-- image.ub

partition2: ext4

root/

rootfilesystem...

 

Here are the command of petalinux we used

$ cd /home/kuma/Desktop/3.7ev_board/projects/20211022

$ petalinux-create -t project -s ../../bsp/uz7ev_evcc_base_2020_2.bsp

 

$ cd /home/kuma/Desktop/3.7ev_board/projects/20211022/uz7ev_evcc_base_2020_2

$ petalinux-config --get-hw-description=/home/kuma/Desktop/3.7ev_board/projects/20211022/ulzd_smcc_tst_wrapper.xsa

 

$ petalinux-build -c avnet-image-full;

 

$ cd images/linux

$ petalinux-package --boot --fsbl zynqmp_fsbl.elf --u-boot u-boot.elf --pmufw pmufw.elf --fpga system.bit --force;

 

$ cp ./BOOT.BIN image.ub boot.scr /media/kuma/boot/

$ sudo dd if=rootfs.ext4 of=/dev/mmcblk0p2

 

Your help is highly appreciated.

Thank you in advance for your help.

Best,

  • Sign in to reply
  • Cancel
Parents
  • kumakichi
    kumakichi over 4 years ago

    Somehow solved.

    The sd card was formatted as

    4MB free space

    5GB(fat32)as boot

    11GB(ext4) as rootfs

    "

    The first partition should be at least 500 MB in size and formatted as a FAT32 file system.

    Ensure that there is 4 MB of free space preceding the partition. The first partition contains

    the boot loader, device tree, and kernel images. Label this partition as BOOT.

    "

    as written in [UG1144 (v2020.2) November 24, 2020] Page107

    in which case the board won't boot up and the PS_OUT_ERR led is red.

     

    then I reformat the sd card and make it as

    5GB(fat32)as boot

    11GB(ext4) as rootfs

     

    this time the board boot and the PS_DONE led turns blue.

     

    Not sure what is happening, hope this would help someone later.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • AshwinRavisankar
    AshwinRavisankar over 4 years ago in reply to kumakichi

    hi kumakichi

    Even i am using the same board and following the same steps, but i get a compile error when i run petalinux-build -c avnet-image-full saying that "amba_pl is missing". How did you go about this error? I havent even declared amba_pl and my hardware design is fairly simple with just a gmii2rgmii converter. Kindly help

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • AshwinRavisankar
    AshwinRavisankar over 4 years ago in reply to AshwinRavisankar

    Also i can share my bit file and the xsa , could you help me build the image files? my project is very straightforward but i cant seem to get it working. I am using ubuntu 18.04 to build and petalinux 2020.2

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • AshwinRavisankar
    AshwinRavisankar over 4 years ago in reply to AshwinRavisankar

    Also i can share my bit file and the xsa , could you help me build the image files? my project is very straightforward but i cant seem to get it working. I am using ubuntu 18.04 to build and petalinux 2020.2