Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Vitis stuck on 67% when running ULTRAZED EV (ultrascale+) application
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 358 subscribers
  • Views 866 views
  • Users 0 members are here
Related

Vitis stuck on 67% when running ULTRAZED EV (ultrascale+) application

Jonathan101
Jonathan101 over 3 years ago
Hi!
I am trying to run simple SPI application om avnet ultrazed EV [with carrier card], after 1 or 2 runs, it stuck at 67%.
I guess the FSBL won't boot, and i need to power cycle. It just make the workflow less efficient..
I know that this problem occur also on ZCU102 board  [which has issues with DDR] 
 
Has someone encounter such a problem, and can instruct me how to fix it?

  • Sign in to reply
  • Cancel
  • shabaz
    shabaz over 3 years ago

    Not based on that level of information.

    You're supposed to troubleshoot, since you have the eyes/ears next to the equipment. Try to come up with simpler solutions that work, and then incrementally build on that, for instance. This is the work an engineer is supposed to do themselves. No-one can do that for you. 

    If your development environment is getting stuck, verify you meet the minimum computer requirements and that you're up-to-date, and so on... If you have already done so, then you should state it. Otherwise people are just guessing, and no-one has time to waste on that (as you can see from the number of responses you have got). You're an engineer, you should know better than to paste this little bit of information and expect a fix.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jonathan101
    Jonathan101 over 3 years ago in reply to shabaz

    Oh I am afraid this is involved DDR and memory issues, and in order to assign that I need time, and expertise which unfortunately I don't have in the moment.

    I check pc requirements and they are fine. Moreover this error is happening randomly. It used to work fine until some change may happen I assume.