Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design PCIe calibration issues on UZ-EV-CC board.
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 358 subscribers
  • Views 2446 views
  • Users 0 members are here
Related

PCIe calibration issues on UZ-EV-CC board.

brianmckee
brianmckee over 3 years ago

With respect to this: https://support.xilinx.com/s/article/72992?language=en_US

Does anyone know if running the latest linux kernel will fix this (2022.2)? Or do I have to update u-boot to the same?

Right now, two PCI cards do not work on the UZ-EV-CC board with this output from linux:

ultrazed ~ # lspci -v
00:00.0 PCI bridge: Xilinx Corporation Device d021 (prog-if 00 [Normal decode])
       Flags: fast devsel, IRQ 255
       Bus: primary=00, secondary=01, subordinate=0c, sec-latency=0
       Memory behind bridge: [disabled] [32-bit]
       Prefetchable memory behind bridge: [disabled] [64-bit]
       Capabilities: [40] Power Management version 3
       Capabilities: [60] Express Root Port (Slot-), MSI 00
       Capabilities: [100] Device Serial Number 00-00-00-00-00-00-00-00
       Capabilities: [10c] Virtual Channel
       Capabilities: [128] Vendor Specific Information: ID=1234 Rev=1 Len=018 <?>

Based on what I found online this sounds like the calibration issue that existed before 2021.X when Xilinx fixed it.

  • Sign in to reply
  • Cancel
Parents
  • brianmckee
    brianmckee over 3 years ago

    I'm looking at the card carrier example design and I'm trying to find the device tree top dts file. I haven't had any luck finding it. Is there documentation on how avnet generates the dts for the card carrier board? Or can someone post the file. I presume it includes zyncmp.dtsi, but it has special gpio devices as well.

    This is all so I can gain control of the dtb file and try to get pcie working.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • brianmckee
    brianmckee over 3 years ago

    I'm looking at the card carrier example design and I'm trying to find the device tree top dts file. I haven't had any luck finding it. Is there documentation on how avnet generates the dts for the card carrier board? Or can someone post the file. I presume it includes zyncmp.dtsi, but it has special gpio devices as well.

    This is all so I can gain control of the dtb file and try to get pcie working.