Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZed-EV TRD
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 475 views
  • Users 0 members are here
  • ask_an_expert
Related

UltraZed-EV TRD

vr00
vr00 over 2 years ago

I was looking into the UltraZed-EV TRD designs and have a few questions:

1.) What is the difference between the hdmi and hdmi_v designs?

2.) I can't seem to get the HDMI Rx to work. I see that there are some scripts in the home directory, but I can't seem to get any of the hdmi scripts to work. (hdmi_passthru.sh, hdmi_to_vcu_to_hdmi.sh, etc).

This is the output I get when running the hdmi_passthru script:

root@uz7ev-evcc-hdmi-v-2023-1:~# ./hdmi_passthrough.sh
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
/GstPipeline:pipeline0/GstKMSSink:kmssink0: display-width = 3840
/GstPipeline:pipeline0/GstKMSSink:kmssink0: display-height = 2160
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
/GstPipeline:pipeline0/GstV4l2Src:v4l2src0.GstPad:src: caps = video/x-raw, framerate=(fraction)60/1, format=(string)UYVY, width=(int)3840, height=(int)2160, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:src: caps = video/x-raw, framerate=(fraction)60/1, format=(string)UYVY, width=(int)3840, height=(int)2160, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709
/GstPipeline:pipeline0/GstKMSSink:kmssink0.GstPad:sink: caps = video/x-raw, framerate=(fraction)60/1, format=(string)UYVY, width=(int)3840, height=(int)2160, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:sink: caps = video/x-raw, framerate=(fraction)60/1, format=(string)UYVY, width=(int)3840, height=(int)2160, pixel-aspect-ratio=(fraction)1/1, interlace-mode=(string)progressive, colorimetry=(string)bt709
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Failed to allocate required memory.
Additional debug info:
/usr/src/debug/gstreamer1.0-plugins-good/1.20.5+gitAUTOINC+48eba62b98-r0/sys/v4l2/gstv4l2src.c(877): gst_v4l2src_decide_allocation (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:
Buffer pool activation failed
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Internal data stream error.
Additional debug info:
/usr/src/debug/gstreamer1.0/1.20.5+gitAUTOINC+48eba62b98-r0/libs/gst/base/gstbasesrc.c(3127): gst_base_src_loop (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:
streaming stopped, reason not-negotiated (-4)
Execution ended after 0:00:00.183210983
Setting pipeline to NULL ...
Freeing pipeline ...
root@uz7ev-evcc-hdmi-v-2023-1:~#

I'm assuming these scripts should be working for each release. Any ideas what I'm doing wrong? Please let me know.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 2 years ago

    (Just guesswork, I don't have this board):

    From your memory error, I'm wondering if maybe the scripts were only tested with non-4K devices (e.g. normal HD, not 4k).

    Or maybe the script accepts display resolution parameters. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 2 years ago

    (Just guesswork, I don't have this board):

    From your memory error, I'm wondering if maybe the scripts were only tested with non-4K devices (e.g. normal HD, not 4k).

    Or maybe the script accepts display resolution parameters.