Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZed EG, IOCC carrier, Petalinux, 2023.1, kernel panic
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 357 subscribers
  • Views 1975 views
  • Users 0 members are here
  • ultrazed-eg
Related

UltraZed EG, IOCC carrier, Petalinux, 2023.1, kernel panic

e2kcpu
e2kcpu over 2 years ago

Hi all,

tried the 2023.1 BSP, looked alright, but booting from SD-CARD, gives a kernel panic:

Zynq MP First Stage Boot Loader
Release 2023.1   May  1 2023  -  00:38:12
PMU Firmware 2023.1    May  1 2023   00:38:12
PMU_ROM Version: xpbr-v8.1.0-0


U-Boot 2023.01 (Mar 29 2023 - 13:08:40 +0000)

CPU:   ZynqMP
Silicon: v3
Chip:  zu3eg
Model: ZynqMP Ultrazed-EG IOCC
Board: Xilinx ZynqMP
DRAM:  2 GiB
PMUFW:    v1.1
PMUFW:  No permission to change config object
EL Level:    EL2
Secure Boot:    not authenticated, not encrypted
Core:  59 devices, 28 uclasses, devicetree: board
NAND:  0 MiB
MMC:   mmc@ff160000: 0, mmc@ff170000: 1
Loading Environment from FAT... *** Error - No Valid Environment Area found
*** Warning - bad env area, using default environment

In:    serial
Out:   serial
Err:   serial
Bootmode: SD_MODE1
Reset reason:    EXTERNAL
Net:   
ZYNQ GEM: ff0e0000, mdio bus ff0e0000, phyaddr 9, interface rgmii-id
eth0: ethernet@ff0e0000
scanning bus for devices...
SATA link 0 timeout.
SATA link 1 timeout.
AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst
starting USB...
Bus usb@fe200000: Register 2000440 NbrPorts 2
Starting the controller
USB XHCI 1.00
scanning bus usb@fe200000 for devices... 1 USB Device(s) found
       scanning usb for storage devices... 0 Storage Device(s) found
Hit any key to stop autoboot:  2  1  0
switch to partitions #0, OK
mmc1 is current device
Scanning mmc 1:1...
Found U-Boot script /boot.scr
563 bytes read in 12 ms (44.9 KiB/s)
## Executing script at 20000000
Trying to boot from SD...
9795716 bytes read in 681 ms (13.7 MiB/s)
## Loading kernel from FIT Image at 04000000 ...
   Using 'conf-system-top.dtb' configuration
   Trying 'kernel-1' kernel subimage
     Description:  Linux kernel
     Created:      2023-04-21   7:47:58 UTC
     Type:         Kernel Image
     Compression:  gzip compressed
     Data Start:   0x04000114
     Data Size:    9750151 Bytes = 9.3 MiB
     Architecture: AArch64
     OS:           Linux
     Load Address: 0x00200000
     Entry Point:  0x00200000
     Hash algo:    sha256
     Hash value:   a5d72d80fd2753ac3422cc85887e8e08a86984261a119cdc25616d4f49b6d9a4
   Verifying Hash Integrity ... sha256+ OK
## Loading fdt from FIT Image at 04000000 ...
   Using 'conf-system-top.dtb' configuration
   Trying 'fdt-system-top.dtb' fdt subimage
     Description:  Flattened Device Tree blob
     Created:      2023-04-21   7:47:58 UTC
     Type:         Flat Device Tree
     Compression:  uncompressed
     Data Start:   0x0494c8ac
     Data Size:    43629 Bytes = 42.6 KiB
     Architecture: AArch64
     Hash algo:    sha256
     Hash value:   4b1526cfc3b3ebc9cefd2cb5a368831dfa762af4e1e31785d8dd8c66d5f6ffaa
   Verifying Hash Integrity ... sha256+ OK
   Booting using the fdt blob at 0x494c8ac
Working FDT set to 494c8ac
Host not halted after 16000 microseconds.
   Uncompressing Kernel Image
   Loading Device Tree to 000000007bbe7000, end 000000007bbf4a6c ... OK
Working FDT set to 7bbe7000

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 6.1.5-xilinx-v2023.1 (oe-user@oe-host) (aarch64-xilinx-linux-gcc (GCC) 12.2.0, GNU ld (GNU Binutils) 2.39.0.20220819) #1 SMP Fri Apr 21 07:47:58 UTC 2023
[    0.000000] Machine model: ZynqMP Ultrazed-EG IOCC
[    0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')
[    0.000000] printk: bootconsole [cdns0] enabled
[    0.000000] efi: UEFI not found.
[    0.000000] Zone ranges:
[    0.000000]   DMA32    [mem 0x0000000000000000-0x000000007fefffff]
[    0.000000]   Normal   empty
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000000000000-0x000000007fefffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000000000000-0x000000007fefffff]
[    0.000000] On node 0, zone DMA32: 256 pages in unavailable ranges
[    0.000000] cma: Reserved 1500 MiB at 0x000000001de00000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] psci: SMC Calling Convention v1.2
[    0.000000] percpu: Embedded 18 pages/cpu s35240 r8192 d30296 u73728
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] alternatives: applying boot alternatives
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 515844
[    0.000000] Kernel command line: console=ttyPS0,115200 earlycon root=/dev/mmcblk1p2 rw rootwait cma=1500M
[    0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[    0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[    0.000000] Memory: 497188K/2096128K available (14528K kernel code, 1024K rwdata, 4136K rodata, 2240K init, 370K bss, 62940K reserved, 1536000K cma-reserved)
[    0.000000] rcu: Hierarchical RCU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=16 to nr_cpu_ids=4.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[    0.000000] Root IRQ handler: gic_handle_irq
[    0.000000] GIC: Using split EOI/Deactivate mode
[    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[    0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0x1ffffffffffffff max_cycles: 0x171015c90f, max_idle_ns: 440795203080 ns
[    0.000001] sched_clock: 57 bits at 100MHz, resolution 10ns, wraps every 4398046511101ns
[    0.008466] Console: colour dummy device 80x25
[    0.012557] Calibrating delay loop (skipped), value calculated using timer frequency.. 199.99 BogoMIPS (lpj=399996)
[    0.022972] pid_max: default: 32768 minimum: 301
[    0.027811] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[    0.034986] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[    0.044088] rcu: Hierarchical SRCU implementation.
[    0.047596] rcu:     Max phase no-delay instances is 1000.
[    0.053101] EFI services will not be available.
[    0.057537] smp: Bringing up secondary CPUs ...
[    0.062323] Detected VIPT I-cache on CPU1
[    0.062397] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[    0.062871] Detected VIPT I-cache on CPU2
[    0.062930] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[    0.063380] Detected VIPT I-cache on CPU3
[    0.063439] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[    0.063491] smp: Brought up 1 node, 4 CPUs
[    0.097529] SMP: Total of 4 processors activated.
[    0.102229] CPU features: detected: 32-bit EL0 Support
[    0.107362] CPU features: detected: CRC32 instructions
[    0.112548] CPU: All CPU(s) started at EL2
[    0.116586] alternatives: applying system-wide alternatives
[    0.123389] devtmpfs: initialized
[    0.130878] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.135214] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[    0.184412] pinctrl core: initialized pinctrl subsystem
[    0.184901] DMI not present or invalid.
[    0.188346] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[    0.194665] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[    0.200888] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.208761] audit: initializing netlink subsys (disabled)
[    0.214213] audit: type=2000 audit(0.152:1): state=initialized audit_enabled=0 res=1
[    0.214628] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.228699] ASID allocator initialised with 65536 entries
[    0.234159] Serial: AMBA PL011 UART driver
[    0.258918] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[    0.260070] HugeTLB: 16380 KiB vmemmap can be freed for a 1.00 GiB page
[    0.266695] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[    0.273477] HugeTLB: 508 KiB vmemmap can be freed for a 32.0 MiB page
[    0.279912] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[    0.286695] HugeTLB: 28 KiB vmemmap can be freed for a 2.00 MiB page
[    0.293048] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[    0.299832] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[    0.374174] raid6: neonx8   gen()  2066 MB/s
[    0.442242] raid6: neonx4   gen()  2031 MB/s
[    0.510312] raid6: neonx2   gen()  1944 MB/s
[    0.578376] raid6: neonx1   gen()  1660 MB/s
[    0.646439] raid6: int64x8  gen()  1297 MB/s
[    0.714506] raid6: int64x4  gen()  1436 MB/s
[    0.782575] raid6: int64x2  gen()  1278 MB/s
[    0.850655] raid6: int64x1  gen()   947 MB/s
[    0.850697] raid6: using algorithm neonx8 gen() 2066 MB/s
[    0.922740] raid6: .... xor() 1513 MB/s, rmw enabled
[    0.922787] raid6: using neon recovery algorithm
[    0.927297] iommu: Default domain type: Translated
[    0.931549] iommu: DMA domain TLB invalidation policy: strict mode
[    0.938041] SCSI subsystem initialized
[    0.941722] usbcore: registered new interface driver usbfs
[    0.947066] usbcore: registered new interface driver hub
[    0.952363] usbcore: registered new device driver usb
[    0.957477] mc: Linux media interface: v0.10
[    0.961679] videodev: Linux video capture interface: v2.00
[    0.967157] pps_core: LinuxPPS API ver. 1 registered
[    0.972089] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.981233] PTP clock support registered
[    0.985163] EDAC MC: Ver: 3.0.0
[    0.988576] zynqmp-ipi-mbox mailbox@ff9905c0: Registered ZynqMP IPI mbox with TX/RX channels.
[    0.997049] FPGA manager framework
[    1.000322] Advanced Linux Sound Architecture Driver Initialized.
[    1.006669] Bluetooth: Core ver 2.22
[    1.009860] NET: Registered PF_BLUETOOTH protocol family
[    1.015157] Bluetooth: HCI device and connection manager initialized
[    1.021510] Bluetooth: HCI socket layer initialized
[    1.026380] Bluetooth: L2CAP socket layer initialized
[    1.031432] Bluetooth: SCO socket layer initialized
[    1.036700] clocksource: Switched to clocksource arch_sys_counter
[    1.042558] VFS: Disk quotas dquot_6.6.0
[    1.046339] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    1.058810] NET: Registered PF_INET protocol family
[    1.058996] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[    1.067105] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[    1.073990] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    1.081719] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[    1.089743] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
[    1.097391] TCP: Hash tables configured (established 16384 bind 16384)
[    1.103554] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[    1.110202] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[    1.117427] NET: Registered PF_UNIX/PF_LOCAL protocol family
[    1.123261] RPC: Registered named UNIX socket transport module.
[    1.128872] RPC: Registered udp transport module.
[    1.133571] RPC: Registered tcp transport module.
[    1.138263] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    1.144706] PCI: CLS 0 bytes, default 64
[    1.149470] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[    1.157729] Initialise system trusted keyrings
[    1.160902] workingset: timestamp_bits=46 max_order=19 bucket_order=0
[    1.167959] NFS: Registering the id_resolver key type
[    1.172318] Key type id_resolver registered
[    1.176462] Key type id_legacy registered
[    1.180476] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    1.187159] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    1.194574] jffs2: version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.
[    1.240811] NET: Registered PF_ALG protocol family
[    1.240862] xor: measuring software checksum speed
[    1.249007]    8regs           :  2311 MB/sec
[    1.253344]    32regs          :  2312 MB/sec
[    1.258006]    arm64_neon      :  2155 MB/sec
[    1.258048] xor: using function: 32regs (2312 MB/sec)
[    1.262842] Key type asymmetric registered
[    1.266929] Asymmetric key parser 'x509' registered
[    1.271833] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[    1.279202] io scheduler mq-deadline registered
[    1.283721] io scheduler kyber registered
[    1.327397] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[    1.329472] Serial: AMBA driver
[    1.337676] brd: module loaded
[    1.341535] loop: module loaded
[    1.345818] tun: Universal TUN/TAP device driver, 1.6
[    1.345967] CAN device driver interface
[    1.349911] usbcore: registered new interface driver rtl8150
[    1.354738] usbcore: registered new interface driver r8152
[    1.360233] usbcore: registered new interface driver asix
[    1.365608] usbcore: registered new interface driver ax88179_178a
[    1.371698] usbcore: registered new interface driver cdc_ether
[    1.377526] usbcore: registered new interface driver net1080
[    1.383186] usbcore: registered new interface driver cdc_subset
[    1.389098] usbcore: registered new interface driver zaurus
[    1.394686] usbcore: registered new interface driver cdc_ncm
[    1.400322] usbcore: registered new interface driver r8153_ecm
[    1.406846] usbcore: registered new interface driver cdc_acm
[    1.411784] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[    1.419957] usbcore: registered new interface driver uas
[    1.425133] usbcore: registered new interface driver usb-storage
[    1.431254] gadgetfs: USB Gadget filesystem, version 24 Aug 2004
[    1.437773] rtc_zynqmp ffa60000.rtc: registered as rtc0
[    1.442340] rtc_zynqmp ffa60000.rtc: setting system clock to 1970-01-01T00:00:04 UTC (4)
[    1.450475] i2c_dev: i2c /dev entries driver
[    1.456718] usbcore: registered new interface driver uvcvideo
[    1.460940] Bluetooth: HCI UART driver ver 2.3
[    1.464860] Bluetooth: HCI UART protocol H4 registered
[    1.469988] Bluetooth: HCI UART protocol BCSP registered
[    1.475310] Bluetooth: HCI UART protocol LL registered
[    1.480428] Bluetooth: HCI UART protocol ATH3K registered
[    1.485839] Bluetooth: HCI UART protocol Three-wire (H5) registered
[    1.492124] Bluetooth: HCI UART protocol Intel registered
[    1.497495] Bluetooth: HCI UART protocol QCA registered
[    1.502730] usbcore: registered new interface driver bcm203x
[    1.508384] usbcore: registered new interface driver bpa10x
[    1.513949] usbcore: registered new interface driver bfusb
[    1.519433] usbcore: registered new interface driver btusb
[    1.524929] usbcore: registered new interface driver ath3k
[    1.530461] EDAC MC: ECC not enabled
[    1.534087] EDAC DEVICE0: Giving out device to module edac controller cache_err: DEV edac (POLLED)
[    1.542902] cortex_edac edac: cortex l1/l2 driver is deprecated
[    1.548992] EDAC DEVICE1: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
[    1.561405] sdhci: Secure Digital Host Controller Interface driver
[    1.567170] sdhci: Copyright(c) Pierre Ossman
[    1.571519] sdhci-pltfm: SDHCI platform and OF driver helper
[    1.577580] ledtrig-cpu: registered to indicate activity on CPUs
[    1.583237] SMCCC: SOC_ID: ID = jep106:0049:0000 Revision = 0x14710093
[    1.589774] zynqmp_firmware_probe Platform Management API v1.1
[    1.595577] zynqmp_firmware_probe Trustzone version v1.0
[    1.630996] securefw securefw: securefw probed
[    1.631332] zynqmp-aes zynqmp-aes.0: will run requests pump with realtime priority
[    1.637993] usbcore: registered new interface driver usbhid
[    1.643026] usbhid: USB HID core driver
[    1.649850] ARM CCI_400_r1 PMU driver probed
[    1.650596] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
[    1.658047] usbcore: registered new interface driver snd-usb-audio
[    1.664612] pktgen: Packet Generator for packet performance testing. Version: 2.75
[    1.672214] Initializing XFRM netlink socket
[    1.675642] NET: Registered PF_INET6 protocol family
[    1.681138] Segment Routing with IPv6
[    1.684198] In-situ OAM (IOAM) with IPv6
[    1.688173] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    1.694422] NET: Registered PF_PACKET protocol family
[    1.699063] NET: Registered PF_KEY protocol family
[    1.703852] can: controller area network core
[    1.708217] NET: Registered PF_CAN protocol family
[    1.712975] can: raw protocol
[    1.715927] can: broadcast manager protocol
[    1.720113] can: netlink gateway - max_hops=1
[    1.724545] Bluetooth: RFCOMM TTY layer initialized
[    1.729337] Bluetooth: RFCOMM socket layer initialized
[    1.734473] Bluetooth: RFCOMM ver 1.11
[    1.738207] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    1.743509] Bluetooth: BNEP filters: protocol multicast
[    1.748732] Bluetooth: BNEP socket layer initialized
[    1.753689] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    1.759608] Bluetooth: HIDP socket layer initialized
[    1.764592] 8021q: 802.1Q VLAN Support v1.8
[    1.768851] 9pnet: Installing 9P2000 support
[    1.773032] Key type dns_resolver registered
[    1.777448] registered taskstats version 1
[    1.781359] Loading compiled-in X.509 certificates
[    1.788567] Btrfs loaded, crc32c=crc32c-generic, zoned=no, fsverity=no
[    1.792810] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa)
[    2.263772] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 24, base_baud = 6249999) is a xuartps
[    2.272868] printk: console [ttyPS0] enabled
[    2.272868] printk: console [ttyPS0] enabled
[    2.277171] printk: bootconsole [cdns0] disabled
[    2.277171] printk: bootconsole [cdns0] disabled
[    2.286624] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 25, base_baud = 6249999) is a xuartps
[    2.300015] gpio gpiochip1: (80000000.gpio): not an immutable chip, please consider fixing it!
[    2.309159] gpio gpiochip3: (80020000.gpio): not an immutable chip, please consider fixing it!
[    2.318020] of-fpga-region fpga-full: FPGA Region probed
[    2.323437] irq-xilinx: mismatch in kind-of-intr param
[    2.328576] irq-xilinx: /amba_pl@0/interrupt-controller@80030000: num_irq=32, sw_irq=0, edge=0x1
[    2.337682] gpio gpiochip4: (zynqmp_gpio): not an immutable chip, please consider fixing it!
[    2.351469] xilinx-zynqmp-dpdma fd4c0000.dma-controller: Xilinx DPDMA engine is probed
[    2.360474] zynqmp-display fd4a0000.display: vtc bridge property not present
[    2.369430] xilinx-dp-snd-codec fd4a0000.display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed
[    2.379522] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed
[    2.387601] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed
[    2.397041] xilinx-dp-snd-card fd4a0000.display:zynqmp_dp_snd_card: Xilinx DisplayPort Sound Card probed
[    2.406622] OF: graph: no port node found in /axi/display@fd4a0000
[    2.413205] xlnx-drm xlnx-drm.0: bound fd4a0000.display (ops 0xffff800008f14788)
[   10.608190] zynqmp-display fd4a0000.display: [drm] Cannot find any crtc or sizes
[   10.615907] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.display on minor 0
[   10.623415] zynqmp-display fd4a0000.display: ZynqMP DisplayPort Subsystem driver probed
[   10.631713] ahci-ceva fd0c0000.ahci: supply ahci not found, using dummy regulator
[   10.639278] ahci-ceva fd0c0000.ahci: supply phy not found, using dummy regulator
[   10.646756] ahci-ceva fd0c0000.ahci: supply target not found, using dummy regulator
[   10.654663] ahci-ceva fd0c0000.ahci: AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl platform mode
[   10.663628] ahci-ceva fd0c0000.ahci: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst
[   10.674196] scsi host0: ahci-ceva
[   10.677826] scsi host1: ahci-ceva
[   10.681274] ata1: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x100 irq 48
[   10.689189] ata2: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x180 irq 48
[   10.697815] spi-nor spi0.0: found n25q256ax1, expected m25p80
[   10.703786] spi-nor spi0.0: n25q256ax1 (32768 Kbytes)
[   10.708966] 3 fixed-partitions partitions found on MTD device spi0.0
[   10.715320] Creating 3 MTD partitions on "spi0.0":
[   10.720109] 0x000000000000-0x000000100000 : "qspi-boot"
[   10.726201] 0x000000100000-0x000001700000 : "qspi-kernel"
[   10.732341] 0x000001700000-0x000001740000 : "qspi-bootenv"
[   10.739131] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
[   10.745689] xilinx-axipmon fd0b0000.perf-monitor: Probed Xilinx APM
[   10.752206] xilinx-axipmon fd490000.perf-monitor: Probed Xilinx APM
[   10.758725] xilinx-axipmon ffa10000.perf-monitor: Probed Xilinx APM
[   10.789839] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[   10.795336] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1
[   10.803089] xhci-hcd xhci-hcd.1.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x0000000002010810
[   10.812502] xhci-hcd xhci-hcd.1.auto: irq 51, io mem 0xfe200000
[   10.818528] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[   10.824012] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2
[   10.831671] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed
[   10.838325] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 6.01
[   10.846586] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[   10.853807] usb usb1: Product: xHCI Host Controller
[   10.858684] usb usb1: Manufacturer: Linux 6.1.5-xilinx-v2023.1 xhci-hcd
[   10.865289] usb usb1: SerialNumber: xhci-hcd.1.auto
[   10.870491] hub 1-0:1.0: USB hub found
[   10.874271] hub 1-0:1.0: 1 port detected
[   10.878539] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 6.01
[   10.886809] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[   10.894036] usb usb2: Product: xHCI Host Controller
[   10.898909] usb usb2: Manufacturer: Linux 6.1.5-xilinx-v2023.1 xhci-hcd
[   10.905525] usb usb2: SerialNumber: xhci-hcd.1.auto
[   10.910732] hub 2-0:1.0: USB hub found
[   10.914503] hub 2-0:1.0: 1 port detected
[   10.919037] cdns-i2c ff030000.i2c: can't get pinctrl, bus recovery not supported
[   10.927457] at24 2-0051: supply vcc not found, using dummy regulator
[   10.934219] at24 2-0051: 256 byte 24c02 EEPROM, writable, 1 bytes/write
[   10.941006] i2c i2c-0: Added multiplexed i2c bus 2
[   10.980711] random: crng init done
[   11.011693] ata2: SATA link down (SStatus 0 SControl 330)
[   11.017116] ata1: SATA link down (SStatus 0 SControl 330)
[   11.369314] i2c i2c-0: Added multiplexed i2c bus 3
[   11.374107] pca954x 0-0070: registered 2 multiplexed busses for I2C switch pca9543
[   11.381724] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 52
[   11.388218] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer with timeout 60s
[   11.395756] cdns-wdt ff150000.watchdog: Xilinx Watchdog Timer with timeout 10s
[   11.403720] macb ff0e0000.ethernet: Not enabling partial store and forward
[   11.414482] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 55 (54:10:ec:67:4f:31)
[   11.427299] of_cfs_init
[   11.429771] of_cfs_init: OK
[   11.433674] ALSA device list:
[   11.436633]   #0: DP mon
[   11.444571] mmc1: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit
[   11.452256] mmc0: SDHCI controller on ff160000.mmc [ff160000.mmc] using ADMA 64-bit
[   11.460062] Waiting for root device /dev/mmcblk1p2...
[   11.493552] mmc1: new high speed SDXC card at address aaaa
[   11.499488] mmcblk1: mmc1:aaaa SN64G 59.5 GiB (ro)
[   11.505971]  mmcblk1: p1 p2
[   11.512792] /dev/root: Can't open blockdev
[   11.516893] VFS: Cannot open root device "mmcblk1p2" or unknown-block(179,2): error -30
[   11.524896] Please append a correct "root=" boot option; here are the available partitions:
[   11.533238] 0100           65536 ram0
[   11.533244]  (driver?)
[   11.539333] 0101           65536 ram1
[   11.539338]  (driver?)
[   11.545432] 0102           65536 ram2
[   11.545437]  (driver?)
[   11.551529] 0103           65536 ram3
[   11.551533]  (driver?)
[   11.557627] 0104           65536 ram4
[   11.557632]  (driver?)
[   11.563724] 0105           65536 ram5
[   11.563729]  (driver?)
[   11.569829] 0106           65536 ram6
[   11.569834]  (driver?)
[   11.575920] 0107           65536 ram7
[   11.575925]  (driver?)
[   11.582019] 0108           65536 ram8
[   11.582024]  (driver?)
[   11.588116] 0109           65536 ram9
[   11.588120]  (driver?)
[   11.594215] 010a           65536 ram10
[   11.594220]  (driver?)
[   11.600397] 010b           65536 ram11
[   11.600402]  (driver?)
[   11.606583] 010c           65536 ram12
[   11.606588]  (driver?)
[   11.612772] 010d           65536 ram13
[   11.612777]  (driver?)
[   11.618954] 010e           65536 ram14
[   11.618958]  (driver?)
[   11.625142] 010f           65536 ram15
[   11.625147]  (driver?)
[   11.631329] 1f00            1024 mtdblock0
[   11.631335]  (driver?)
[   11.637871] 1f01           22528 mtdblock1
[   11.637876]  (driver?)
[   11.644397] 1f02             256 mtdblock2
[   11.644402]  (driver?)
[   11.650930] b300        62367744 mmcblk1
[   11.650935]  driver: mmcblk
[   11.657726]   b301         1048576 mmcblk1p1 f8f46eba-01
[   11.657732]
[   11.664517]   b302         3332919 mmcblk1p2 f8f46eba-02
[   11.664522]
[   11.671308] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)
[   11.679734] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 6.1.5-xilinx-v2023.1 #1
[   11.686858] Hardware name: ZynqMP Ultrazed-EG IOCC (DT)
[   11.692067] Call trace:
[   11.694497]  dump_backtrace.part.0+0xc0/0xd0
[   11.698767]  show_stack+0x18/0x30
[   11.702074]  dump_stack_lvl+0x6c/0x88
[   11.705728]  dump_stack+0x18/0x34
[   11.709035]  panic+0x164/0x31c
[   11.712082]  mount_block_root+0x18c/0x238
[   11.716084]  mount_root+0x208/0x244
[   11.719564]  prepare_namespace+0x130/0x170
[   11.723653]  kernel_init_freeable+0x26c/0x294
[   11.728001]  kernel_init+0x28/0x130
[   11.731482]  ret_from_fork+0x10/0x20
[   11.735051] SMP: stopping secondary CPUs
[   11.738961] Kernel Offset: disabled
[   11.742436] CPU features: 0x00000,01000100,0000420b
[   11.747306] Memory Limit: none
[   11.750348] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2) ]---

SD-Card looks OK:

emu@HP803:~$ ll /SD1
total 16644
drwxr-xr-x  2 root root    4096 Dec 31  1969 ./
drwxr-xr-x 28 root root    4096 Jun 18 13:06 ../
-rwxr-xr-x  1 root root 7231224 Apr  5  2011 boot.bin*
-rwxr-xr-x  1 root root     563 Apr  5  2011 boot.scr*
-rwxr-xr-x  1 root root 9795716 Apr  5  2011 image.ub*
emu@HP803:~$ ll /SD2
total 88
drwxr-xr-x 19 root root  4096 Jun 20 11:21 ./
drwxr-xr-x 28 root root  4096 Jun 18 13:06 ../
drwxr-xr-x  2 root root  4096 Mar  9  2018 bin/
drwxr-xr-x  2 root root  4096 Mar  9  2018 boot/
drwxr-xr-x  2 root root  4096 Mar  9  2018 dev/
drwxr-xr-x 60 root root  4096 Mar  9  2018 etc/
drwxr-xr-x  4 root root  4096 Mar  9  2018 home/
drwxr-xr-x  8 root root  4096 Mar  9  2018 lib/
drwx------  2 root root 16384 Jun 20 11:21 lost+found/
drwxr-xr-x  2 root root  4096 Mar  9  2018 media/
drwxr-xr-x  2 root root  4096 Mar  9  2018 mnt/
dr-xr-xr-x  2 root root  4096 Mar  9  2018 proc/
drwxr-xr-x  2 root root  4096 Mar  9  2018 run/
drwxr-xr-x  2 root root  4096 Mar  9  2018 sbin/
drwxr-xr-x  2 root root  4096 Mar  9  2018 srv/
dr-xr-xr-x  2 root root  4096 Mar  9  2018 sys/
drwxrwxrwt  2 root root  4096 Mar  9  2018 tmp/
drwxr-xr-x 13 root root  4096 Mar  9  2018 usr/
drwxr-xr-x  9 root root  4096 Mar  9  2018 var/

What am I missing?

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • dyessgg
    dyessgg over 2 years ago

    Found it.  Add the following to your system-user.dtsi.  This was from a slightly older version of Petalinux so the dtsi file name might have changed since then.

    /* SD1 with level shifter */
    &sdhci1
    {    status = "OK";
        max-frequency = <50000000>;
        disable-wp;    // Required for uSD without write protect signal
        no-1-8-v;    /* for 1.0 silicon */
    };

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e2kcpu
    e2kcpu over 2 years ago in reply to dyessgg

    Sorry to be so stupid, but which is the correct system-user.dtsi file to use?

    I see in my source tree five of them ...

    4 ./components/yocto/layers/meta-petalinux/dynamic-layers/xilinx-tools/recipes-bsp/uboot-device-tree/files/system-user.dtsi
    4 ./components/yocto/layers/meta-petalinux/dynamic-layers/xilinx-core/recipes-bsp/device-tree/files/system-user.dtsi
    4 ./project-spec/decoupling-dtsi/system-user.dtsi
    4 ./project-spec/meta-user/recipes-bsp/device-tree/files/system-user.dtsi
    4 ./project-spec/meta-user/meta-xilinx-tools/recipes-bsp/uboot-device-tree/files/system-user.dtsi

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dyessgg
    dyessgg over 2 years ago in reply to e2kcpu

    They have changed some things since 2022.  The first 3 are definitely NOT where you want it.  I'm thinking the 4th one, recipes-bsp is the correct place.  Just make sure it's a file that is not overwritten when you do a new hardware import.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e2kcpu
    e2kcpu over 2 years ago in reply to dyessgg

    Now I have a different(?) problem?

    [    1.695056] Bluetooth: RFCOMM TTY layer initialized
    [    1.699845] Bluetooth: RFCOMM socket layer initialized
    [    1.704979] Bluetooth: RFCOMM ver 1.11
    [    1.708708] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
    [    1.714016] Bluetooth: BNEP filters: protocol multicast
    [    1.719239] Bluetooth: BNEP socket layer initialized
    [    1.724195] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
    [    1.730114] Bluetooth: HIDP socket layer initialized
    [    1.735099] 8021q: 802.1Q VLAN Support v1.8
    [    1.739361] 9pnet: Installing 9P2000 support
    [    1.743536] Key type dns_resolver registered
    [    1.747957] registered taskstats version 1
    [    1.751866] Loading compiled-in X.509 certificates
    [    1.759083] Btrfs loaded, crc32c=crc32c-generic, zoned=no, fsverity=no
    [    1.763309] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa)
    [    2.234326] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 24, base_baud = 6249999) is a xuartps
    [    2.243418] printk: console [ttyPS0] enabled
    [    2.243418] printk: console [ttyPS0] enabled
    [    2.247722] printk: bootconsole [cdns0] disabled
    [    2.247722] printk: bootconsole [cdns0] disabled
    [    2.257164] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 25, base_baud = 6249999) is a xuartps
    [   26.924751] rcu: INFO: rcu_sched self-detected stall on CPU
    [   26.930313] rcu:     0-....: (5249 ticks this GP) idle=143c/1/0x4000000000000000 softirq=73/73 fqs=2625
    [   26.939442]  (t=5250 jiffies g=-1083 q=8 ncpus=4)
    [   26.944142] CPU: 0 PID: 155 Comm: kworker/u8:2 Not tainted 6.1.5-xilinx-v2023.1 #1
    [   26.951698] Hardware name: ZynqMP Ultrazed-EG IOCC (DT)
    [   26.956908] Workqueue: edac-poller edac_device_workq_function
    [   26.962653] pstate: 20000005 (nzCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
    [   26.969605] pc : smp_call_function_single+0xd4/0x190
    [   26.974570] lr : cortex_arm64_edac_check+0xbc/0x190
    [   26.979439] sp : ffff80000ae1bcb0
    [   26.982738] x29: ffff80000ae1bcb0 x28: 0000000000000000 x27: ffff0000029d3700
    [   26.989864] x26: 00000000000000a0 x25: 0000000000000004 x24: 0000000000000030
    [   26.996991] x23: ffff800008a493d0 x22: ffff8000095d91d0 x21: ffff8000094999e0
    [   27.004117] x20: ffff800009499ba0 x19: ffff80000ae1bce0 x18: 0000000000000000
    [   27.011243] x17: ffff80000951e1e8 x16: 0000000000000000 x15: 0000000000000001
    [   27.018370] x14: 0000000000000000 x13: 0000000000000000 x12: 0000000000000003
    [   27.025496] x11: 0000000000000000 x10: ffff80000ae1bd68 x9 : ffff80000ae1bd60
    [   27.032622] x8 : ffff80000ae1bd78 x7 : 000000000000000f x6 : ffff800008a493d0
    [   27.039749] x5 : 0000000000000000 x4 : ffff00007fa775c8 x3 : 0000000000000001
    [   27.046875] x2 : 0000000000000000 x1 : ffff00007fa775c0 x0 : 0000000000000003
    [   27.054002] Call trace:
    [   27.056433]  smp_call_function_single+0xd4/0x190
    [   27.061041]  cortex_arm64_edac_check+0xbc/0x190
    [   27.065563]  edac_device_workq_function+0x84/0xe0
    [   27.070259]  process_one_work+0x1fc/0x380
    [   27.074261]  worker_thread+0x74/0x4b0
    [   27.077915]  kthread+0xd8/0xdc
    [   27.080962]  ret_from_fork+0x10/0x20
    [   27.084530] Task dump for CPU 2:
    [   27.087742] task:kworker/u8:0    state:R  running task     stack:0     pid:8     ppid:2      flags:0x0000000a
    [   27.097645] Workqueue: events_unbound deferred_probe_work_func
    [   27.103469] Call trace:
    [   27.105900]  __switch_to+0xe4/0x160
    [   27.109381]  0xffff0000018b6100

    It seems to be the location, where it does access the GPIO?

    [    2.272868] printk: console [ttyPS0] enabled
    [    2.272868] printk: console [ttyPS0] enabled
    [    2.277171] printk: bootconsole [cdns0] disabled
    [    2.277171] printk: bootconsole [cdns0] disabled
    [    2.286624] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 25, base_baud = 6249999) is a xuartps
    [    2.300015] gpio gpiochip1: (80000000.gpio): not an immutable chip, please consider fixing it!
    [    2.309159] gpio gpiochip3: (80020000.gpio): not an immutable chip, please consider fixing it!
    [    2.318020] of-fpga-region fpga-full: FPGA Region probed
    [    2.323437] irq-xilinx: mismatch in kind-of-intr param
    [    2.328576] irq-xilinx: /amba_pl@0/interrupt-controller@80030000: num_irq=32, sw_irq=0, edge=0x1
    [    2.337682] gpio gpiochip4: (zynqmp_gpio): not an immutable chip, please consider fixing it!
    [    2.351469] xilinx-zynqmp-dpdma fd4c0000.dma-controller: Xilinx DPDMA engine is probed
    [    2.360474] zynqmp-display fd4a0000.display: vtc bridge property not present
    [    2.369430] xilinx-dp-snd-codec fd4a0000.display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed
    [

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e2kcpu
    e2kcpu over 2 years ago in reply to dyessgg

    Now I have a different(?) problem?

    [    1.695056] Bluetooth: RFCOMM TTY layer initialized
    [    1.699845] Bluetooth: RFCOMM socket layer initialized
    [    1.704979] Bluetooth: RFCOMM ver 1.11
    [    1.708708] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
    [    1.714016] Bluetooth: BNEP filters: protocol multicast
    [    1.719239] Bluetooth: BNEP socket layer initialized
    [    1.724195] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
    [    1.730114] Bluetooth: HIDP socket layer initialized
    [    1.735099] 8021q: 802.1Q VLAN Support v1.8
    [    1.739361] 9pnet: Installing 9P2000 support
    [    1.743536] Key type dns_resolver registered
    [    1.747957] registered taskstats version 1
    [    1.751866] Loading compiled-in X.509 certificates
    [    1.759083] Btrfs loaded, crc32c=crc32c-generic, zoned=no, fsverity=no
    [    1.763309] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa)
    [    2.234326] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 24, base_baud = 6249999) is a xuartps
    [    2.243418] printk: console [ttyPS0] enabled
    [    2.243418] printk: console [ttyPS0] enabled
    [    2.247722] printk: bootconsole [cdns0] disabled
    [    2.247722] printk: bootconsole [cdns0] disabled
    [    2.257164] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 25, base_baud = 6249999) is a xuartps
    [   26.924751] rcu: INFO: rcu_sched self-detected stall on CPU
    [   26.930313] rcu:     0-....: (5249 ticks this GP) idle=143c/1/0x4000000000000000 softirq=73/73 fqs=2625
    [   26.939442]  (t=5250 jiffies g=-1083 q=8 ncpus=4)
    [   26.944142] CPU: 0 PID: 155 Comm: kworker/u8:2 Not tainted 6.1.5-xilinx-v2023.1 #1
    [   26.951698] Hardware name: ZynqMP Ultrazed-EG IOCC (DT)
    [   26.956908] Workqueue: edac-poller edac_device_workq_function
    [   26.962653] pstate: 20000005 (nzCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
    [   26.969605] pc : smp_call_function_single+0xd4/0x190
    [   26.974570] lr : cortex_arm64_edac_check+0xbc/0x190
    [   26.979439] sp : ffff80000ae1bcb0
    [   26.982738] x29: ffff80000ae1bcb0 x28: 0000000000000000 x27: ffff0000029d3700
    [   26.989864] x26: 00000000000000a0 x25: 0000000000000004 x24: 0000000000000030
    [   26.996991] x23: ffff800008a493d0 x22: ffff8000095d91d0 x21: ffff8000094999e0
    [   27.004117] x20: ffff800009499ba0 x19: ffff80000ae1bce0 x18: 0000000000000000
    [   27.011243] x17: ffff80000951e1e8 x16: 0000000000000000 x15: 0000000000000001
    [   27.018370] x14: 0000000000000000 x13: 0000000000000000 x12: 0000000000000003
    [   27.025496] x11: 0000000000000000 x10: ffff80000ae1bd68 x9 : ffff80000ae1bd60
    [   27.032622] x8 : ffff80000ae1bd78 x7 : 000000000000000f x6 : ffff800008a493d0
    [   27.039749] x5 : 0000000000000000 x4 : ffff00007fa775c8 x3 : 0000000000000001
    [   27.046875] x2 : 0000000000000000 x1 : ffff00007fa775c0 x0 : 0000000000000003
    [   27.054002] Call trace:
    [   27.056433]  smp_call_function_single+0xd4/0x190
    [   27.061041]  cortex_arm64_edac_check+0xbc/0x190
    [   27.065563]  edac_device_workq_function+0x84/0xe0
    [   27.070259]  process_one_work+0x1fc/0x380
    [   27.074261]  worker_thread+0x74/0x4b0
    [   27.077915]  kthread+0xd8/0xdc
    [   27.080962]  ret_from_fork+0x10/0x20
    [   27.084530] Task dump for CPU 2:
    [   27.087742] task:kworker/u8:0    state:R  running task     stack:0     pid:8     ppid:2      flags:0x0000000a
    [   27.097645] Workqueue: events_unbound deferred_probe_work_func
    [   27.103469] Call trace:
    [   27.105900]  __switch_to+0xe4/0x160
    [   27.109381]  0xffff0000018b6100

    It seems to be the location, where it does access the GPIO?

    [    2.272868] printk: console [ttyPS0] enabled
    [    2.272868] printk: console [ttyPS0] enabled
    [    2.277171] printk: bootconsole [cdns0] disabled
    [    2.277171] printk: bootconsole [cdns0] disabled
    [    2.286624] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 25, base_baud = 6249999) is a xuartps
    [    2.300015] gpio gpiochip1: (80000000.gpio): not an immutable chip, please consider fixing it!
    [    2.309159] gpio gpiochip3: (80020000.gpio): not an immutable chip, please consider fixing it!
    [    2.318020] of-fpga-region fpga-full: FPGA Region probed
    [    2.323437] irq-xilinx: mismatch in kind-of-intr param
    [    2.328576] irq-xilinx: /amba_pl@0/interrupt-controller@80030000: num_irq=32, sw_irq=0, edge=0x1
    [    2.337682] gpio gpiochip4: (zynqmp_gpio): not an immutable chip, please consider fixing it!
    [    2.351469] xilinx-zynqmp-dpdma fd4c0000.dma-controller: Xilinx DPDMA engine is probed
    [    2.360474] zynqmp-display fd4a0000.display: vtc bridge property not present
    [    2.369430] xilinx-dp-snd-codec fd4a0000.display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed
    [