Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Clock Generator 2 – U6, IDT 8T49N241-048NLGI on Ultrazed-ev board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 358 subscribers
  • Views 1518 views
  • Users 0 members are here
  • clock
  • ultrazed-ev
Related

Clock Generator 2 – U6, IDT 8T49N241-048NLGI on Ultrazed-ev board

Jonathan101
Jonathan101 over 1 year ago

Hi,

I changed the frequency of the output clocks in U6 on Ultrazed-ev development board using i2c interface in clock 2 test header.

Is it possible to reset the output clocks in U6 back to default?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 1 year ago

    Here is what you are looking for. You will see a text file here that need to be programmed to the EEPROM.

    https://github.com/Avnet/petalinux/tree/master/configs/meta-user/uz7ev_evcc_factest/recipes-apps/eeprom-test/files

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jonathan101
    Jonathan101 over 1 year ago in reply to e14 Contributor

    Hi,

    Do you or some of Avnet board have the updated .tcs file that is required by Renesas software 'timing ocmmander' to program the 8T49N241?

    I wasn't able to program it using the .txt file from git

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bidrohini
    bidrohini over 1 year ago

    If the clock configuration you modified was stored only in volatile memory (RAM), simply powering off the UltraZed-EV and then powering it back on will restore the default clock settings.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • iksevas
    iksevas over 1 year ago in reply to Jonathan101

    I'm not certain that you can use TIMING COMMANDER to physically program the EEPROM which is necessary to maintain the configuration. Suggestion is to use the TXT file from GITHUB and have the processor use I2C commands and program the TXT file to the EEPROM.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jonathan101
    Jonathan101 over 1 year ago in reply to iksevas

    Can you elaborate on how to use the processor to do so?

    You mean I should place xilinx i2c ip core on vivado and connect it to i2c_data and i2c_clk of the eeprom?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • iksevas
    iksevas over 1 year ago in reply to Jonathan101

    If you use the UltraZed-EV BSP, the I2C should already be available for you.

    The clock generator U6 is programmed by the EEPROM U5. The CC_SCL/SDA signals are tied to the Carrier Card SOM connectors which maps to an I2C MUX on the SOM, U8. The I2C MUX is fed by the processor I2C interface using MIO24/25 (I2C1 interface).

    The I2C MUX should be programmed to drive traffic to port 0 of the MUX (the CC_SCL/SDA port). You would potentially need some I2C transfers to set this to port 0 if it doesn't default there. The I2C address for this MUX is on the SOM schematic, 0xE0.

    Once traffic is set to CC_SCL/SDA, then you need to write the text file data to the U5 EEPROM. The I2C address for the U5 EEPROM is on the Carrier Card schemtic, 0xA4.

    The Avnet GITHUB has I2C EEPROM examples already. It could just be a matter of reviewing that code and substituting/modifying the code to support the transfer of the text file data.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • James123
    James123 over 1 year ago

    Yes, you can reset the output clock of U6 to its default value. The 8T49N241 originally supports programming through the I2C interface.