Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design UltraZED-EV with FMC-SDI card to have 4KP60 via SDI (input and output)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 358 subscribers
  • Views 423 views
  • Users 0 members are here
Related

UltraZED-EV with FMC-SDI card to have 4KP60 via SDI (input and output)

danielsan77
danielsan77 over 1 year ago

Hello!
I'm using the UltraZED-EV (SOM + Carrier) for a project where I need to process 4KP60 video on the FPGA (PL-side).

To do this, we'll be working with the SDI input (4KP60) and the SDI output (4KP60), and I need both the SDI input and SDI output to go to the PL-side, so I can process the 4KP60 video there (in the PL-side).

To summarize, please answer the following two questions:
1. Which FMC-SDI cards do you recommend that are compatible with UltraZed-EV (SOM + Carrier) and allow us to have 4KP60 over SDI (12G-SDI, input and output)? I've seen some FMC-SDI cards, but I'm not sure if they're compatible.
2. Do the SDI signals from the FMC-SDI card go through the PL side of the FPGA (I don't want to use the PS side) of the UltraZED-EV (SOM + Carrier)?

Thank you very much!
Daniel.

  • Sign in to reply
  • Cancel
Parents
  • iksevas
    0 iksevas over 1 year ago

    I don’t know of FMC SDI card. Your search is as good as mine. UltraZed-EV g bc as 3g-SDi on board Carrier Card. This supports 1080P60.

    So, you will only be able to get 4KP60 with a compatible FMC card and you will be limited to that FMC card to get that performance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • danielsan77
    0 danielsan77 over 1 year ago in reply to iksevas

    Thanks for answering!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • danielsan77
    0 danielsan77 over 1 year ago in reply to iksevas

    Thanks for answering!