Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Ultrazed Hardware Design Is CAN connection possible with UltraZed EG IO carrier card?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 629 views
  • Users 0 members are here
  • ultrazed-eg
  • io carrier card
  • can
Related

Is CAN connection possible with UltraZed EG IO carrier card?

kimitsuda
kimitsuda over 7 years ago

The IO carrier card has only one PS PMOD connector, to which MIO 36-43 of Zynq MPSoC is connected.

How can I use this connector to perform CAN communication with the CAN controller in the Zynq PS?

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    drozwood90 over 7 years ago

    Unlike USB, you can use EMIO to bring this out to just about any connector.

     

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kimitsuda
    kimitsuda over 7 years ago in reply to drozwood90

    Thanks for the comment, Dan.

     

    I understand that any PL_PMOD connector can be used via EMIO.

    By the way, this IO carrier card seems to have Level-Translator installed, but it seems that CAN-bus transceiver is not installed.

    Is CAN communication possible with this IO carrier board?

     

    For example, in ZCU102, it is as follows.

    "The PS-side CAN bus TX and RX MIO pins go through TXS0104E level-translator U33 and TI SN65HVD232 CAN-bus transceiver U122 before being presented to the user 0.1 inch centered 8-pin male header J98"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kimitsuda
    kimitsuda over 7 years ago in reply to drozwood90

    Thanks for the comment, Dan.

     

    I understand that any PL_PMOD connector can be used via EMIO.

    By the way, this IO carrier card seems to have Level-Translator installed, but it seems that CAN-bus transceiver is not installed.

    Is CAN communication possible with this IO carrier board?

     

    For example, in ZCU102, it is as follows.

    "The PS-side CAN bus TX and RX MIO pins go through TXS0104E level-translator U33 and TI SN65HVD232 CAN-bus transceiver U122 before being presented to the user 0.1 inch centered 8-pin male header J98"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • drozwood90
    drozwood90 over 7 years ago in reply to kimitsuda

    Hi there,

     

    If you need to add a transceiver or something else, you are free to use the PMOD ports to expand the board.  If you need a CAN transceiver, you could for example use this PMOD:

    https://store.digilentinc.com/pmod-can-can-2-0b-controller-with-integrated-transceiver/

     

    --Dan