Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Rev D ZedBoard Schematic/BOM Posted
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 5016 views
  • Users 0 members are here
Related

Rev D ZedBoard Schematic/BOM Posted

bhfletcher
bhfletcher over 13 years ago

ZedBoard has been updated with a few minor corrections as well as now being built with production Zynq silicon. This new revision is Rev D.2. The schematics and BOM for this new revision are now posted in the Documentation area. A complete change list from C.1 to D.2 is on the last page of the schematics.

 

http://www.zedboard.org/documentation

 

Bryan

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi,
    the last page of the D.2 schematics says:
    PCB: add series termination resistor to SD Clock.
    Parts: load new resistor with 50ohm resistor.
    But on page 6 there is no risistor to find.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 13 years ago

    The 50-ohm series termination resistor is on the Zynq side. This is R293 on Sheet 10 of the schematics.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Did you repair the wrongly dimensioned 1V line, which will lead to unstableness when using the PL?
    ( http://www.zedboard.org/content/1v-power-supply-under-powered )

    Did you repair the EMC/ESD-problem, when you connect the Zedboard ground to whatever grounded device (Ethernet, USB, ...) or get anykind of ESD-spike - the Zedbord will reset?
    ( http://www.zedboard.org/content/zedboard-resets-upon-connecting-usb-or-ethernet )

    Did you repair the awful leaking powersupply which you provide with the Zedboard, providing +80volts related to mains earth to the zedboards ground, leading to destructed I/O-pins of the FPGA sooner or later?

    The quality of the Zedboard is very far from what I have used to with Xilinx boards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 13 years ago in reply to e14 Contributor

    It sounds like you may be better suited to the ZC702 board -- www.xilinx.com/zc702

     

    The 1V supply is capable of delivering 2A. This was not redesigned on Rev D. We believe 2A is sufficient for most users.

     

    The EMC/ESD problem was not resolved on the first batch of Rev D board but will be fixed moving forward. The fix is not that difficult and is detailed in the ZedBoard Errata as well as Sam Bobrowicz' response in the original post.

     

    Regarding the power supply, please see Sam Bobrowicz' response in the original post.
    http://www.zedboard.org/content/zedboard-resets-upon-connecting-usb-or-ethernet

    Bryan