Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Custom ip (AXi streaming protocol) for dma
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 358 subscribers
  • Views 310 views
  • Users 0 members are here
Related

Custom ip (AXi streaming protocol) for dma

Former Member
Former Member over 12 years ago

Hi there,

i've been successful at creating different kind of IPs, mostly in AXi lite etc..
I would like to implement DMA in the zynq and i could need some help:
   DMA streams of data from FPGA to CPU

I have gathered many tutorials & stuff but i still am not able to implement a streaming IP to create a DMA transfer, could some one explain me how to proceed at connecting everything?



If i got it right:
we need to use the streaming protocol (might be even easier than AXi lite, fewer signals);

We need to use a DMA IP from the IP catalog and it seems the DMA engine would be the one, but i still hesitate with CDMA. The only difference which makes me tend to use DMA engine is that it has a Bus Interface allowing connexion to what should be a custom IP while the other doesn't have any. May be wrong?

So we add the DMA IP from catalog.
Then we have two options:
  ACP: accelerator coherent port to transfer data to the MEMORY CACHE
  HP high perf port to transfer data to DDR RAM (better?)

tend to use the HP options
then i need two HP one for write one for read. We can modify the accessible addresses which, as i understand it, will be the addresses inside the DDR RAM.