Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Video Processing with Vivado HLS block on Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 353 subscribers
  • Views 554 views
  • Users 0 members are here
Related

Video Processing with Vivado HLS block on Zedboard

Former Member
Former Member over 11 years ago

Hi,

I am trying to create a simple video processing system using the zedboard and the FMC Imageon card. I implemented the passthrough reference design "FMC-IMAGEON IP Cores and Tutorials for Vivado" and it is working. Then I created my own IP Block using Vivado HLS. The first version of my block was only a passthrough function. The function just got the input image and sent it to the ouput. I synthetized and exported the IP and integrated to the passthrough reference design using Vivado IP Integrator. I put it after the VideoIn-to-AXIStream and before the AXIStream-to-VideoOut. All this worked very well. I got the video from a camera using the FMC HDMI input port and got video out to a monitor. My problem is the following: Then I wanted to create a more complicated function in my HLS design so I used one of the video processing library functions, a sobel filter, and repeated the process again. I exported the IP block and add it in the middle of the passthrough example, however this DOESN'T WORK! My guess is that it has something to do with the clocks or the timing. Maybe the sobel filter is too slow or something like that. Do you have any idea what could be wrong? I don't get anything in the screen when using the sobel filter block. My HDMI input is 720p. I am using a clock of 150MHz to run my block but I also tried with 75Mhz and still. You can find my documents here: http://community.em.avnet.com/avnet/attachments/avnet/FMCHDMIIOVITAImageSensor/297/1/Sobel_Filter_Project_Files.zip

Any idea or suggestion. I don't know what is going on. I'll appreciate your quick response.

Thanks,

Manuel

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    Hi, Could you pls kindly tell me what is the FMC imageon card that you are using?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago

    Hi, Could you pls kindly tell me what is the FMC imageon card that you are using?