Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design PS I2C on Xillinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 360 subscribers
  • Views 1593 views
  • Users 0 members are here
Related

PS I2C on Xillinux

e14 Contributor
e14 Contributor over 13 years ago

Hi,
I use Xillinux and I need I2C for my application.
I open system.xmp, enable I2C 0 in PS and configure to use MIO 10..11. I folow instuctions in Getting started with Xillinux for Zynq-7000 EPP 3.3, 3.5 and 3.6. New bitstreem is identical to origin. I thing that bitstreem must be little different.
What I do wrong?

Thanks

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I take look at http://www.zedboard.org/content/zedboard-out-box-sd-card-image-and-source.
    Looks like, the MIO configuration is stored in the FSBL.
    Is it right?
    How can I modifi FSBL?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I have some progress. FSBL is possible to create from SDK. I tried to add UART0 and I2C0 both connected to the MIO. I adjusted DTS. UART works well, but I2C is still not accessible from linux. /dev/i2c-0 does not exists.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Vatu,

    Did you recompile Linux and create the dtb file form the ./scripts directory based on your updated dts file?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    There are two ways to come around this:

    (1) If you don't need the card's sound capability, and you're fine with using PL pins from the chip, you may "steal" the I2C interface used to program the sound chip. Just reLOC the relevant pins to your application logic, and disable the sound subsystem as described in the Getting Started Guide for Linux.

    (2) If you want the native I2C Linux driver to run the relevant PL lines, you'll need to modify the DTS file, and compile it into a DTB, and then copy it to the SD card's first partition. The entry you need to add tells the kernel that an I2C hardware element is available, and also its attributes. I've never done this, but this is the flow. There shouldn't be a need to recompile the kernel, I believe.

       Eli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Thanks for answer.
    I decompile DTB on first partition of SD using DTC -I dtb -O dts -o devicetree.dts devicetree.dtb. I add UART0 and I2C0 in to DTS. Last step is compiling DTB using DTC -I dts -O dtb -o devicetree.dtb devicetree.dts. Uart works fine but I2C does not.

    Two possible reasons:
    1. Wrong entry for I2C0 in DTS
    2. Driver for I2C not found or does not exist in Xillinux.

    I am linux newbie and I am not sure how to verify this.
    I tried list modules by lsmod and modprobe -l. But nothing look like I2C driver. I thing that I2C driver is not instaled. I believe that it is not need recompile entire kernel. I read in  "Getting started with Xillybus on a Linux host" about compiling single module respective specified folder. This is what I tryed, but no success yet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I think choose 2 is right way.

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi Tim,
    I am recompile kernel. I am use git clone https://github.com/Digilent/linux-3.3-digilent.git to get sources. I am apply 6 patches from /usr/src/xillinux/kernel-patches successfly. I am recompile kernel using by make. Then I copy zImage from arch/arm/boot to first partition on SD.

    I am decompile DTB on first partition of SD using DTC -I dtb -O dts -o devicetree.dts devicetree.dtb. I add UART0 and I2C0 in to DTS.

    ttserial@e0000000 {
    tttclock = <0x2faf080>;
    tttcompatible = "xlnx,ps7-uart-1.00.a", "xlnx,xuartps";
    tttdevice_type = "serial";
    tttinterrupt-parent = <0x1>;
    tttinterrupts = <0x0 0x1b 0x0>;
    tttreg = <0xe0000000 0x1000>;
    tttxlnx,has-modem = <0x0>;
    tttxlnx,uart-clk-freq-hz = <0x2faf080>;
    tt};


    tti2c0: i2c@e0004000 {
    tttcompatible = "xlnx,ps7-i2c-1.00.a";
    tttreg = <0xE0004000 0x1000>;
    tttinterrupts = <0 25 0>;
    tttinterrupt-parent = <1>;
    tttbus-id = <0>;
    tttinput-clk = <50000000>;
    ttti2c-clk = <100000>;
    ttt
    ttt#address-cells = <1>;
    ttt#size-cells = <0>;
    tt};

    Last step is compiling DTB using DTC -I dts -O dtb -o devicetree.dtb devicetree.dts.

    After power off and power on zedboard boot successfly.





    U-Boot 2012.04.01 (Oct 16 2012 - 17:41:50)

    DRAM:  512 MiB
    WARNING: Caches not enabled
    MMC:   SDHCI: 0
    Using default environment

    In:    serial
    Out:   serial
    Err:   serial
    Net:   zynq_gem
    Hit any key to stop autoboot:  0
    Copying Linux from SD to RAM...
    Device: SDHCI
    Manufacturer ID: 1d
    OEM: 4144
    Name: SD
    Tran Speed: 25000000
    Rd Block Len: 512
    SD version 2.0
    High Capacity: Yes
    Capacity: 15 GiB
    Bus Width: 4-bit
    reading zImage

    2674504 bytes read
    reading devicetree.dtb

    6483 bytes read
    reading ramdisk8M.image.gz

    ** Unable to read "ramdisk8M.image.gz" from mmc 0:1 **
    ## Starting application at 0x00008000 ...
    Uncompressing Linux... done, booting the kernel.
    [    0.000000] Booting Linux on physical CPU 0
    [    0.000000] Linux version 3.3.0-xillinux-1.0+ (root@arbot2) (gcc version 4.6.3 (Ubuntu/Linaro 4.6.3-1ubuntu5) ) #1 SMP PREEMPT Sat Nov 10 20:54:10 UTC 2012
    [    0.000000] CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    [    0.000000] Machine: Xilinx Zynq Platform, model: Xillinux for Zedboard
    [    0.000000] bootconsole [earlycon0] enabled
    [    0.000000] Memory policy: ECC disabled, Data cache writealloc
    [    0.000000] BUG: mapping for 0xf8f00000 at 0xfe00c000 out of vmalloc space
    [    0.000000] BUG: mapping for 0xe0000000 at 0xfe000000 out of vmalloc space
    [    0.000000] BUG: mapping for 0xffff1000 at 0xfe200000 out of vmalloc space
    [    0.000000] PERCPU: Embedded 7 pages/cpu @c09c0000 s5440 r8192 d15040 u32768
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 125824
    [    0.000000] Kernel command line: consoleblank=0 root=/dev/mmcblk0p2 rw rootwait earlyprintk
    [    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
    [    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
    [    0.000000] Memory: 240MB 256MB = 496MB total
    [    0.000000] Memory: 497428k/497428k available, 26860k reserved, 0K highmem
    [    0.000000] Virtual kernel memory layout:
    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    [    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    [    0.000000]     vmalloc : 0xe0800000 - 0xfd000000   ( 456 MB)
    [    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
    [    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    [    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
    [    0.000000]       .text : 0xc0008000 - 0xc04bf650   (4830 kB)
    [    0.000000]       .init : 0xc04c0000 - 0xc04e9540   ( 166 kB)
    [    0.000000]       .data : 0xc04ea000 - 0xc051bfa0   ( 200 kB)
    [    0.000000]        .bss : 0xc051bfc4 - 0xc0538028   ( 113 kB)
    [    0.000000] Preemptible hierarchical RCU implementation.
    [    0.000000]  Verbose stalled-CPUs detection is disabled.
    [    0.000000] NR_IRQS:128
    [    0.000000] xlnx,ps7-ttc-1.00.a #0 at 0xe0800000, irq=43
    [    0.000000] Console: colour dummy device 80x30
    [    0.000000] console [tty0] enabled, bootconsole disabled

    Ubuntu 12.04 LTS arbot2 ttyPS0

    arbot2 login: root (automatic login)

    Last login: Sun Nov 11 08:00:07 UTC 2012 from 192.168.10.100 on pts/1
    Welcome to the Xillinux distribution for Zynq-7000 EPP.

    You may communicate data with standard FPGA FIFOs in the logic fabric by
    writing to or reading from the /dev/xillybus_* device files. Additional
    pipe files of that sort can be set up at request of a custom Xillybus IP core.

    For more information: http://www.xillybus.com.

    To start a graphical X-Windows session, type "startx" at shell prompt.



    But without i2c. :-(
    i2cdetect -l returns nothing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I found log entry in /var/log/dmesg

    [    1.430000] xi2cps e0004000.i2c: 100 kHz mmio e0004000 irq 57

    But /dev/i2c-0 still does not exists.
    I have no idea.
    Any suggestions?

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Solved. It is easy. I2C-dev module must be installed (by default is disabled). It is controlled by option CONFIG_I2C_CHARDEV in .config.


    Vatu

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    There is detailed procedure how to get working PS I2C.

    http://www.arbot.cz/post/2012/11/14/PS-I2C-in-Xillinux.aspx


    Vatu

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>