Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design SFP Card for ZedBoard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 1175 views
  • Users 0 members are here
Related

SFP Card for ZedBoard

Former Member
Former Member over 11 years ago

Hello,
I saw that Xilinx sells SFP FMC Cards for the ZC702 Board.
http://www.xilinx.com/products/boards_kits/fmc.htm#SERIAL

The ZC702 has the same SoC as your ZedBoard. So my question is:
Is it possible to design a SFP FMC Card by my own for the ZedBoard? Respectively, which ports do I have to use?

Thanks in advance

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 11 years ago

    The Zynq XC7Z020 device that is on the ZedBoard and the ZC702 board does not have any high speed transceivers, so neither would support a SFP FMC Card. While the SFP FMC (HPC) Card might physically fit onto the ZC702 FMC (LPC) connector I believe the table indicating the SFP FMC Card is compatible with the ZC702 is in error.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Thank you for your quick response!

    If I would design a SFP FMC Card with a PHY on it like the MAX24287 (http://www.microsemi.com/documents/clock/ds/MAX24287_short_form_2012-08.pdf), it should work or not? This PHY has a RGMII Interface as output, so I think I can put it on nearly every FMC pin, is this correct?

    Thank you Gary!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago

    The Zynq device on the ZedBoard has two GigaBit Etherenet controllers in the Processing Subsystem. By default one of them is connected directly to the PHY on the ZedBoard via MIO pins using the RGMII interface. Assuming you want to keep this Ethernet interface you could connect the remaining controller to the Zynq Programmable Logic (PL) section via EMIO to a GMII interface that could then be connected to the FMC connector.

     

    If you want two Ethernet interfaces you would have to disable the MIO to RGMII interface to the on-board PHY and route it via EMIO to another GMII interface or implement a 'soft' GigaBit ethernet controller in the PL for the second port. It will be up to you to verify that you have enough connections available from the Zynq device to the FMC connector to accomplish this.

     

    There are existing boards that use Zynq devices with high speed transceivers that already of SFP connections such as the Mini-ITX board:  http://zynqgeek.zedboard.org/product/mini-itx

    and the Zynq MMP board with a MMP BaseBoard II: http://zynqgeek.zedboard.org/product/mmp-baseboard-II.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Thanks again Gary,
    one SFP interface is absolutly enaugh for me.

    Greetings from Germany

    Micha

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer