Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zedboard/AD-FMCOMMS2-EBZ reference design crashes ISE 14.4
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 360 subscribers
  • Views 347 views
  • Users 0 members are here
Related

Zedboard/AD-FMCOMMS2-EBZ reference design crashes ISE 14.4

e14 Contributor
e14 Contributor over 12 years ago

I am using the reference design from https://github.com/analogdevicesinc/fpgahdl_xilinx.git (using git clone) with ISE 14.4 (64 bit RHEL 6 version). I am using the procedure to generate xilinx netlist files from xco (from http://wiki.analog.com/resources/eval/user-guides/ad-fmcomms2-ebz/refere...). When I import "cf_lib/edk/pcores/adi_common_v1_00_a/netlist/ad_dcfilter_1.xco", ISE 14.4 crashes with the following message:

"FATAL_ERROR:GuiUtilities:Gui_Clip_ApplicationBase.c:369:1.30 - No index entry
for empty element ID. This application has performed an illegal operation and
must be shut down. Process will terminate. For technical support on this
issue, please open a WebCase with this project attached at
http://www.xilinx.com/support."

Do you have recommendations to address this problem? The problem occurs both with and without the update to ISE 14.4.

Thanks,
Arun

P.S: Reposting in a new thread, in case my previous message was lost as a reply.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    When I try to import "cf_lib/edk/pcores/adi_common_v1_00_a/netlist/ad_dcfilter_1.xco" in Win 7, I get the error: "A Xilinx application has encountered an unexepcted error... No index entry for empty element ID."

    In the Information tab, there is a message "ERROR:sim:879 - Part'xc7z020-1clg484' is not valid for component 'xilinx.com:ip:xbip_dsp48_macro:2.0'.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    The problem with the dsp48 macro is a show stopper for Zedboard and ISE, because, per Xilinx documentation, the first dsp48 macro version that works with Zynq is v3.0, which is tested with Vivado, not ISE. Can you please let me know if there is an actual working implementation for Zedboard with either ISE or Vivado?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    The problem with the dsp48 macro is a show stopper for Zedboard and ISE, because, per Xilinx documentation, the first dsp48 macro version that works with Zynq is v3.0, which is tested with Vivado, not ISE. Can you please let me know if there is an actual working implementation for Zedboard with either ISE or Vivado?