Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zedboard - VGA
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 360 subscribers
  • Views 627 views
  • Users 0 members are here
Related

Zedboard - VGA

metinburak_
metinburak_ over 11 years ago

The analog VGA connector is directly connected to the digital Zynq pins. Why isn't there any VGA DAC? How come is VGA interface implemented by digital pins?

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 11 years ago

    Hi metinburak,

    The ZedBoard VGA connector is connected to the Zynq device via a R-2R resistor ladder configuration which gives 4-bits of resolution per color channel on the VGA interface.  Take a look at this Wikipedia entry to better understand this configuration:

    http://en.wikipedia.org/wiki/Resistor_ladder

    This is an implementation that the folks at Digilent have implemented on several development boards to avoid the cost of an additional VGA DAC chip.  There is an ISE based reference design project published on the Digilent ZedBoard product page which implements a test pattern generator out the VGA interface:

    http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,400,1028&Prod=ZEDBOARD

    Also, the folks at Xillybus have this VGA interface working with their Xillinux distribution so that may be another resource that is useful to you:

    http://xillybus.com/xillinux

    If you need better than VGA resolutions or wider than 4-bit per channel color space, I recommend looking at using the ADV7511 HDMI output on ZedBoard instead of VGA since there is more material available which covers the use of HDMI within a Vivado design.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • metinburak_
    0 metinburak_ over 11 years ago

    Is there any other way in this HW configuration to make VGA better (or wider channel) using VHDL?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer