Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design UART No output on serial termination
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 450 views
  • Users 0 members are here
Related

UART No output on serial termination

e14 Contributor
e14 Contributor over 12 years ago

Hi all,

I have a bera metal video system( parallel video input -> Vid_in_axi4s -> VDMA -> Memory), and i found the Status register of VDMA gives Error status(at this time, UART can output on the termination)u3002 To debug it, i add chipscope (axi_monitor/ila) to my project, but when i run the software, this time there is No any output on the serial termination!  Does chipscope affect the UART1?  Very confusion! How can i fix this problemuFF01 Any suggestion would be very appreciate!   (ISE 14.5) 
 
Best Regards,
Dec

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Then I try to debug the code to check whether the UART1 in an abnormal status in SDK. But when i switch to DEBUG perspective,
    i can not resume the code as it is inactive(grey status). Step In, Step Out, Step Over, Step Return are the same status.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 12 years ago

    I'm not sure what is happening, but adding chipscope should have no affect on the UART. The latest public driver from Cypress has disabled the persistent mode on the COM port. Therefore, when you cycle power to the ZedBoard, you must disconnect the terminal, and then reconnect after the system is powered up again.

    Bryan