Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Problem when connecting custom IP with AXI streaming interface generated by Vivado to AXI interconnect bus via AXI DMA engine
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 298 views
  • Users 0 members are here
Related

Problem when connecting custom IP with AXI streaming interface generated by Vivado to AXI interconnect bus via AXI DMA engine

e14 Contributor
e14 Contributor over 13 years ago

Hi, all,
  I generate a custom IP with AXI streaming interface using Vivado. My software function is like
-----------------------------------------
  fun test (int input1[4][4], int input2[4][4], int output[4][4] ) {};
-----------------------------------------
It takes two input matrice and produces one output matrix. So I choose the streaming interface.

When I connect my custom ip to the processing system, there is an error:
-----------------------------------------
ERROR:EDK - processing_system7_0 (processing_system7) - C_S_AXI_HP2_HIGHADDR has an allowable range of 0x00000000 to 0x1FFFFFFF.
Address Map for Processor processing_system7_0
(0x40400000-0x4040ffff) axi_dma_0 axi_interconnect_1
(0x40440000-0x4044ffff) axi_dma_1 axi_interconnect_1
(0x72800000-0x7280ffff) fixed_point_top_0 axi_interconnect_1
-----------------------------------------

Here is the link of my screen shot of the system connection. (also attached the system.mhs file)
(Because The function has 2 input matrix and I don't know how can one DMA support two MM2S interface, I build 2 DMA engines for each input matrix)

https://docs.google.com/file/d/0B-mwYWFYhKwBanhPZ2lrQnhkQ2s/edit?usp=sharing
https://docs.google.com/file/d/0B-mwYWFYhKwBWlI1Q3FSRldKdEE/edit?usp=sharing

My target board is Zedboard.
Software version is Xilinx 14.2

Can anyone give me some direction?
Thanks.
Henry

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi
    I am interested in your project.
    If you solved it, can you teach me how to handle it?

    thanks