Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Gigabit Ethernet
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 442 views
  • Users 0 members are here
Related

Gigabit Ethernet

Former Member
Former Member over 13 years ago


Hi,

1) How to transfer DDR3/BRAM data to PC via Gigabit Ethernet?

2) What are the available C libraries to implement Gigabit Ethernet on ZedBoard with ARM processor?

3) Is there any reference design available for Gigabit Ethernet implementation on ZedBoard with ARM processor?

Thank you.

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 13 years ago

    samarawickrama,

    1.  There are a number of ways to get data from the DDR3/BRAM to a PC.  If you are running on bare-metal (no Operating System) you can use Light Weight IP Stack (LWIP) which is provided for you as a free library within SDK.  If you are running Linux, you can just use the standard C libraries to write a C program, or any other language you prefer.

    If you just have a dataset (say a char array) then you can easily just point LWIP to the array and send it out.  I believe LWIP also supports jumbo frames.

    2.  See my answer to #1.

    3.  I do not know of any at the moment.  If you are using Linux you can use any number of examples written for that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer