Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zedboard FMC connector replacement
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 360 subscribers
  • Views 493 views
  • Users 0 members are here
Related

Zedboard FMC connector replacement

cyb_at
cyb_at over 11 years ago

The FMC connector on the Zedboard I have "broke" by accident. I had an extension board sitting on the FMC connector. The Zedboard fell (by accident) and landed on the connected extension board. As such this ended up partially ripping the FMC connector out of the Zedboard.

1. Since the FMC connector is partially rippped, should I just remove it instead of trying to putting it back onto the board? OR Can I replace the FMC connector or solder it back? If so, any recommendation on how?

2. Can I still use the remaining of the board if I am not interfacing with the damaged FMC connector?

Any help will be appreciated.

Thanks.

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Here is what our engineering group had to say:

     

    If the connector "ripped" partially off the board he may have lifted the pads, in which case the board cannot be repaired.

     

    He needs to:

     - Have the Connector removed with heat

     - Clean any remaining solder off the pads.

     - Inspect the pads on PCB with a microscope to see if any of them are lifted.  If any of them are obviously lifted then no need for the microscope.

     

    If the pads are still in-tact then he can order a new connector and have it placed back on the board by a local CM. A stencil will need to be ordered for them to palace the new connector.

     

    The rest of the board should operate fine with the damaged connector.

     

    Hope that was helpful. I suspect that replacing the board might be more cost effective than repair.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cyb_at
    0 cyb_at over 11 years ago in reply to Former Member

    Thanks for the response Gary.

    Yes the pads are busted. I can use the board for other application where I do not need a FMC connector. I shall get a new board. It will surely be cheaper that trying to repair it.

    Thank you for the help. I appreciate it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer