Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design 1V Power supply under-powered
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 15 replies
  • Subscribers 361 subscribers
  • Views 2220 views
  • Users 0 members are here
Related

1V Power supply under-powered

e14 Contributor
e14 Contributor over 13 years ago

What's the maximum power that can by drawn by the Zynq PL? Has this been tested?

I have build a large design (80%) that need to runs at 100MHz, but when I program the bitstream to the Zedboard. The Zynq reset a few ms after being DONE.

Also, I have probed the 1V power supply at C357. After, the PL is DONE, the voltage go down to about 560mV and go back up to 1V probably because the PL resets.

What could be causing this?

Is it because the PL draw to much power?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I though I'd let you know that I have confirmed this issue.

    I bypassed the 1V power supply by using an external power supply. Now, the design is working and as much as 3A is drawn from the 1V power supply.

    This is much more than the 2A the MAX15021ATI+ (onboard 1V PSU) is capable of.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I have the similar issue and need an external power supply to power the core voltage. Any tips in modifying the board? Where did you cut the wire and connect the jumper wires? Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I have the similar issue and need an external power supply to power the core voltage. Any tips in modifying the board? Where did you cut the wire and connect the jumper wires? Thanks.