Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design 1V Power supply under-powered
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 15 replies
  • Subscribers 360 subscribers
  • Views 2213 views
  • Users 0 members are here
Related

1V Power supply under-powered

e14 Contributor
e14 Contributor over 13 years ago

What's the maximum power that can by drawn by the Zynq PL? Has this been tested?

I have build a large design (80%) that need to runs at 100MHz, but when I program the bitstream to the Zedboard. The Zynq reset a few ms after being DONE.

Also, I have probed the 1V power supply at C357. After, the PL is DONE, the voltage go down to about 560mV and go back up to 1V probably because the PL resets.

What could be causing this?

Is it because the PL draw to much power?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Using the zedboard for cryptographic applications, I experienced the power limit on the 1V Vccint and it is really a killer. In this kind of application, you try to fill up the FPGA and to use every clock cycle.

    I don't want to sound grumpy - I enjoy my zedboard very much - but I do think this limitation should be either corrected or clearly advertised otherwise people might just buy a useless board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Using the zedboard for cryptographic applications, I experienced the power limit on the 1V Vccint and it is really a killer. In this kind of application, you try to fill up the FPGA and to use every clock cycle.

    I don't want to sound grumpy - I enjoy my zedboard very much - but I do think this limitation should be either corrected or clearly advertised otherwise people might just buy a useless board.