Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Maximum frequency xillinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 360 subscribers
  • Views 869 views
  • Users 0 members are here
Related

Maximum frequency xillinux

deaxman
deaxman over 12 years ago

Hi, I've heard it said that the maximum frequency that the zedboard can reach is dependant upon the quality of your code.  What does this mean?  If I am using the xillydemo.v file from the xillinux installation, how do I figure out what the maximum frequency is (besides trial and error) and how do I increase this maximum frequency?  Code "quality" is very subjective.  I feel that the maximum would be less dependant on efficiency of your code and more dependant on the number of resources that are being used.  Thanks!

  • Sign in to reply
  • Cancel
Parents
  • deaxman
    0 deaxman over 12 years ago

    Thanks!  This answers pretty much everything!  When testing these clocks I would send them out of the pmod (w12) and check them with the o-scope.  At 250 and 300 (MHz) I still see the occilation but it doesn't get up to the 3.3v that one would expect.  Do this mean that this clock will also fail to register as a "high" on the internal logic or is it simply poor propagation through the pmod (I looked and see that the pmod vtc are not perfectly ideal, there are delays and attenuations)  It seems that if any ocillation can be seen then it must be going high and low within the logic and it's just having trouble when it tries to enforce that high or low on the pmod output.  I am using gclk or clk_100 which is the 100mhz internal clk.  What documentation should I look at to check this out?  I will look into taking the course, it sounds like a great option but it would be great if I could figure this out quickly and then come to a more long term solution through the course.  Thanks!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • deaxman
    0 deaxman over 12 years ago

    Thanks!  This answers pretty much everything!  When testing these clocks I would send them out of the pmod (w12) and check them with the o-scope.  At 250 and 300 (MHz) I still see the occilation but it doesn't get up to the 3.3v that one would expect.  Do this mean that this clock will also fail to register as a "high" on the internal logic or is it simply poor propagation through the pmod (I looked and see that the pmod vtc are not perfectly ideal, there are delays and attenuations)  It seems that if any ocillation can be seen then it must be going high and low within the logic and it's just having trouble when it tries to enforce that high or low on the pmod output.  I am using gclk or clk_100 which is the 100mhz internal clk.  What documentation should I look at to check this out?  I will look into taking the course, it sounds like a great option but it would be great if I could figure this out quickly and then come to a more long term solution through the course.  Thanks!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data