Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design External PMOD pin Grounding
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 366 views
  • Users 0 members are here
Related

External PMOD pin Grounding

e14 Contributor
e14 Contributor over 12 years ago

Hi All

I am trying to connect up a ADC to the PMOD connections on the ZedBoard but am having trouble with the output pins connections. Through an oscilloscope the pins don't look like they are being driven properly. An output pin takes about 2 seconds to reach 3.3V once toggled.

My XDC file is as follows for each pin.

set_property PACKAGE_PIN "W12" [get_ports "TRIG"]
set_property IOSTANDARD "LVCMOS33" [get_ports "TRIG"]
set_property PIO_DIRECTION "OUTPUT" [get_ports "TRIG"]
set_property slew "fast" [get_ports "TRIG"]
set_property drive "8" [get_ports "TRIG"]

...

If anyone has any suggestions or a list of steps to interface to these pins please let me know.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello Alex,

     

    I set up a simple Zedboard design in Vivado 2013.3 with an AXI_GPIO output to the PMOD pin JB1 (W12), first with the simple XDC constraints:

     

    set_property package_pin w12 [get_ports TRIG]

    set_property iostandard lvcmos33 [get_ports TRIG]

     

    Then wrote a simple program in SDK to drive the signal high and low using Xil_Out32. It seems to toggle high and low just fine, with sharp edges and at a rate of ~ 200 nsec. per level change. I added in your other XDC constraints with the same results. I am monitoring the JB1 pin with no load and it is swinging from 0v to 3.3v.

     

    Are you seeing a slow rise time that might indicate the load is more than the 8 mA can drive or an actual 2 sec. delay with a sharp rising edge?

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer