Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design AD-FMCOMMS1-EBZ Zedboard problems with a custom design
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 539 views
  • Users 0 members are here
Related

AD-FMCOMMS1-EBZ Zedboard problems with a custom design

Former Member
Former Member over 12 years ago

Hi,

I'm working with a Zedboard and I have correctly implemented the reference design from here:
http://wiki.analog.com/resources/eval/user-guides/ad-fmcomms1-ebz/reference_hdl

Now I'm interested in creating my own design from the reference design. I have just removed the modules HDMI, spdif, GPIO and modified the DTS file but I still cannot communicate with the board AD-FMCOMMS1-EBZ. I attach the response I get when booting Linaro Linux OS through a SD card:



U-Boot 2012.04.01 (Jun 26 2013 - 11:27:41)

DRAM:  512 MiB
WARNING: Caches not enabled
MMC:   SDHCI: 0
Using default environment

In:    serial
Out:   serial
Err:   serial
Net:   zynq_gem
Hit any key to stop autoboot:  0
Copying Linux from SD to RAM...
Device: SDHCI
Manufacturer ID: 73
OEM: 4247
Name: NCard
Tran Speed: 25000000
Rd Block Len: 512
SD version 2.0
High Capacity: Yes
Capacity: 7.5 GiB
Bus Width: 4-bit
reading zImage

2795528 bytes read
reading devicetree.dtb

8646 bytes read
reading ramdisk8M.image.gz

** Unable to read "ramdisk8M.image.gz" from mmc 0:1 **
## Starting application at 0x00008000 ...
Uncompressing Linux... done, booting the kernel.
Booting Linux on physical CPU 0
Linux version 3.6.0 (srivas@PW7I-4-D-367) (gcc version 4.6.3 (Sourcery CodeBench Lite 2012.03-79) ) #1 SMP PREEMPT Wed Jun 26 11:11:09 CEST 2013
CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Xilinx Zynq Platform, model: Xilinx Zynq ZC702
bootconsole [earlycon0] enabled
cma: CMA: reserved 40 MiB at 1d800000
Memory policy: ECC disabled, Data cache writealloc
PERCPU: Embedded 7 pages/cpu @c0e59000 s7872 r8192 d12608 u32768
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048
Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait devtmpfs.mount=0
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 512MB = 512MB total
Memory: 468060k/468060k available, 56228k reserved, 0K highmem
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    vmalloc : 0xe0800000 - 0xff000000   ( 488 MB)
    lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    modules : 0xbf000000 - 0xbfe00000   (  14 MB)
      .text : 0xc0008000 - 0xc04cc1b8   (4881 kB)
      .init : 0xc04cd000 - 0xc04f4ec0   ( 160 kB)
      .data : 0xc04f6000 - 0xc05466a0   ( 322 kB)
       .bss : 0xc05466c4 - 0xc0a4d750   (5149 kB)
Preemptible hierarchical RCU implementation.
tRCU lockdep checking is enabled.
tDump stacks of tasks blocking RCU-preempt GP.
tRCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
NR_IRQS:512
MIO pin 11 not assigned(00001760)
xslcr mapped to e0802000
Zynq clock init
timer #0 at e0804000, irq=43
sched_clock: 32 bits at 100 Hz, resolution 10000000ns, wraps every 4294967286ms
Console: colour dummy device 80x30
Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo Molnar
... MAX_LOCKDEP_SUBCLASSES:  8
... MAX_LOCK_DEPTH:          48
... MAX_LOCKDEP_KEYS:        8191
... CLASSHASH_SIZE:          4096
... MAX_LOCKDEP_ENTRIES:     16384
... MAX_LOCKDEP_CHAINS:      32768
... CHAINHASH_SIZE:          16384
memory used by lock dependency info: 3695 kB
per task-struct memory footprint: 1152 bytes
Calibrating delay loop... 1332.01 BogoMIPS (lpj=6660096)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
Setting up static identity map for 0x360ec0 - 0x360ef4
L310 cache controller enabled
l2x0: 8 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x72360000, Cache size: 524288 B
CPU1: Booted secondary processor
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
Brought up 2 CPUs
SMP: Total of 2 processors activated (2664.03 BogoMIPS).
devtmpfs: initialized
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Advanced Linux Sound Architecture Driver Version 1.0.25.
Switching to clocksource xttcps_clocksource
NET: Registered protocol family 2
TCP established hash table entries: 16384 (order: 5, 131072 bytes)
TCP bind hash table entries: 16384 (order: 7, 589824 bytes)
TCP: Hash tables configured (established 16384 bind 16384)
TCP: reno registered
UDP hash table entries: 256 (order: 2, 20480 bytes)
UDP-Lite hash table entries: 256 (order: 2, 20480 bytes)
NET: Registered protocol family 1
msgmni has been set to 994
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
xuartps e0001000.uart: failed to get alias id, errno -19
e0001console [ttyPS0] enabled, bootconsole disabled
console [ttyPS0] enabled, bootconsole disabled
xdevcfg f8007000.devcfg: ioremap f8007000 to e080e000 with size 1000
[drm] Initialized drm 1.1.0 20060810
brd: module loaded
loop: module loaded
libphy: XEMACPS mii bus: probed
xemacps e000b000.eth: pdev->id -1, baseaddr 0xe000b000, irq 54
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
xusbps-dr e0002000.usb: Unable to init USB phy, missing?
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mousedev: PS/2 mouse device common for all mice
i2c /dev entries driver
at24 0-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write
at24 0-0054: 256 byte 24c02 EEPROM, writable, 1 bytes/write
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: Invalid maximum block size, assuming 512 bytes
mmc0: SDHCI controller on e0100000.sdhci [e0100000.sdhci] using ADMA
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
mmc0: new high speed SDHC card at address b368
mmcblk0: mmc0:b368 NCard 7.48 GiB
cf_axi_adc 79020000.cf-ad9643-core-lpc: Device Tree Probing 'cf-ad9643-core-lpc'
platform 79020000.cf-ad9643-core-lpc: Driver cf_axi_adc requests probe deferral
spi spi32766.1: Driver ad9467 requests probe deferral
mmcblk0: p1 p2
spi_master spi32766: failed to transfer one message from queue
iio iio:device0: write failed (-110)
ad8366: probe of spi32766.6 failed with error -110
spi_master spi32766: failed to transfer one message from queue
ad9548: probe of spi32766.2 failed with error -110
spi_master spi32766: failed to transfer one message from queue
iio iio:device0: write failed (-110)
ad9523: probe of spi32766.3 failed with error -110
ERROR: could not get clock /amba@0/i2c@41600000/spi_xcomm0@58/adf4351-rx-lpc@4:clkin(0)
spi spi32766.4: Driver adf4350 requests probe deferral
ERROR: could not get clock /amba@0/i2c@41600000/spi_xcomm0@58/adf4351-tx-lpc@5:clkin(0)
spi spi32766.5: Driver adf4350 requests probe deferral
cf_axi_dds 74200000.cf-ad9122-core-lpc: Device Tree Probing 'cf-ad9122-core-lpc'
platform 74200000.cf-ad9122-core-lpc: Driver cf_axi_dds requests probe deferral
spi_master spi32766: failed to transfer one message from queue
ad9122 spi32766.0: Unrecognized CHIP_ID 0xFFFFFF92
TCP: cubic registered
NET: Registered protocol family 17
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
Registering SWP/SWPB emulation handler
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
cf_axi_adc 79020000.cf-ad9643-core-lpc: Device Tree Probing 'cf-ad9643-core-lpc'
platform 79020000.cf-ad9643-core-lpc: Driver cf_axi_adc requests probe deferral
spi spi32766.1: Driver ad9467 requests probe deferral
ERROR: could not get clock /amba@0/i2c@41600000/spi_xcomm0@58/adf4351-rx-lpc@4:clkin(0)
spi spi32766.4: Driver adf4350 requests probe deferral
ERROR: could not get clock /amba@0/i2c@41600000/spi_xcomm0@58/adf4351-tx-lpc@5:clkin(0)
spi spi32766.5: Driver adf4350 requests probe deferral
cf_axi_dds 74200000.cf-ad9122-core-lpc: Device Tree Probing 'cf-ad9122-core-lpc'
platform 74200000.cf-ad9122-core-lpc: Driver cf_axi_dds requests probe deferral
ALSA device list:
  No soundcards found.
EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:2.
Freeing init memory: 156K
init: ureadahead main process (717) terminated with status 5
Last login: Thu Jan  1 00:00:10 UTC 1970 on tty1
Welcome to Linaro 12.09 (GNU/Linux 3.6.0 armv7l)

How can I solve the problem of the SPI communication?
How does it affect my design when removing any hardware module from the reference design?

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    Thank you so much DSP_1!!!
    The problem was the IRQ numbers in the DTS file. I was going crazy, I could not see that detail before. So thank you very much for showing me the light ;).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago

    Thank you so much DSP_1!!!
    The problem was the IRQ numbers in the DTS file. I was going crazy, I could not see that detail before. So thank you very much for showing me the light ;).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data