Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design zedborad ddr3 dq delay
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 358 subscribers
  • Views 272 views
  • Users 0 members are here
Related

zedborad ddr3 dq delay

e14 Contributor
e14 Contributor over 10 years ago

Hi all,
 When I read the Zedborad_HW_UG_V2.0.pdf,I found the Propagaton delay of the DQ[7..0] is 160ps/inch(Table 2 -DDR3 Worksheet Calculations).
 Also I found the signals of DQ[7..0] are not in the same layer (Gibber file of the zedboard),for example the dq2 is in the top layer and the dq4 is in the Third layer mainly.
  The propagaton delay of the trace in the top layer and in third layer is not the same. I calculare the delay time according to the pcb information of zedboard.  The propagaton delay in the top layer is 149ps/inch and  in third layer is 173ps/inch. Also the dq4 has two holes and each adds about 17ps delay。if we assume the net length of the dq2 and dq4 are equal,then the delay time of dq4 and dq2 is (173-149)*netlength + 17ps*2. The netlength is about 51mm,so the dalay time between the dq2 and dq4 is about 80ps.
  Could someone tell me why the zedboard is still working well and  what is the max skew of the dq group of the zedboard.
 
   thank you
   

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 10 years ago

    What is the delay time of dq2 and dq4 relative to dqs? That is the critical measurement. Also, keep in mind that using a faster grade memory than what you are running gives you additional leeway. See Appendix A in UG933. For example, a 1600 memory running at 1066 on a Zynq rated at 1066 gives you a dq allowed skew of +/-73ps relative to dqs.

    Bryan