Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Trouble Connecting A Second SD Card to Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 358 subscribers
  • Views 290 views
  • Users 0 members are here
Related

Trouble Connecting A Second SD Card to Zedboard

e14 Contributor
e14 Contributor over 11 years ago

I can see how the Fixed SD Card is connected to the SDIO0 block in the PS using MIO pins 40-47. I would like to connected a second SD Card using the PModSD from Digilent directly to the SDIO1 block in the PS by plugging it into the MIO PMOD (JE1).

I have come to the conclusion that Digilent's PModSD is not compatible with the MIO PMOD (JE1). Using JE1 and PModSD, the mappings are fixed (SD-func <-> PMod pin# <-> MIO#) but incorrect. For example, the SD-cmd is connected to PMod pin #2, which in turn connects to MIO_10. The only SDIO1 pin which MIO_10 connects to is IO-Bit0, but the SD-cmd signal needs to be connected to Command pin, which is only accessible through MIO_11.

I feel that I might be missing something, since this use-case seems fairly obvious. I I can see how I might connect the PModSD to the SDIO1 controller on the PS using EMIO and one of PMods connected to the PL. The reason I want to avoid this is that I am already short on PMod connections to the PL...

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 11 years ago

    Because of the fixed nature of the pinout for both the Pmod standard as well as the PS peripherals, it was impossible to create a pinout that would satisfy all the PS peripherals with all the possible Pmods.

     

    The easy solution is to use flywires to make the correct connections. Go to http://digilentinc.com/Products/Catalog.cfm?NavPath=2,393&Cat=3. Purchase a 2x6 Pin Header, which you install in the Pmod. Then purchase a few packs of 1 Pin MTE Cables. Then you can connect the Pmod with the correct pinout.

     

    Bryan