Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design DRAM components
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 683 views
  • Users 0 members are here
Related

DRAM components

Former Member
Former Member over 10 years ago

Hi,

According to ZedBoard_HW_UG_v1_1.pdf, the ZedBoard includes two Micron DDR3 memory components.

In the application I'm developing I need to read and write arrays in RAM, so I wonder if it is possible to use one of the memory components for writing and the other for reading, reading and writing need to be performed in parallel.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 10 years ago

    Hello Emanuel,

     

    The Zynq PS DDR Memory Controller is detailed in UG585, the Zynq 7000 Technical Reference Manual, in Chapter 10:

     

    http://www.xilinx.com/support/documentation/user_guides/ug585-Zynq-7000-TRM.pdf

     

    While it can implement either a 16 bit or a 32 bit physical interface to the external DDR memory devices there is no option to implement two separate 16 bit interfaces. You can issue 'parallel' read and write requests and the DDR controller will queue them up and execute them as efficiently as possible.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago

    Hello Emanuel,

     

    The Zynq PS DDR Memory Controller is detailed in UG585, the Zynq 7000 Technical Reference Manual, in Chapter 10:

     

    http://www.xilinx.com/support/documentation/user_guides/ug585-Zynq-7000-TRM.pdf

     

    While it can implement either a 16 bit or a 32 bit physical interface to the external DDR memory devices there is no option to implement two separate 16 bit interfaces. You can issue 'parallel' read and write requests and the DDR controller will queue them up and execute them as efficiently as possible.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
No Data