Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design enable SPI
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 354 subscribers
  • Views 492 views
  • Users 0 members are here
Related

enable SPI

ashahsana
ashahsana over 10 years ago

Hello everyone
I am new in this field, I try to find out how can I enable spidev. I already saw that in the SPI is active in the xilinx_zynq_defconfig file.
Can anyone guide me how can I enable Spidev ???
I am using 7z020 board.
regards
one update Now i know I have to change my dts file but how?

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 10 years ago

    Hi Sana,

    Are you hooking up the PL AXI QSPI controller?  If so, take a look at this thread here:

    https://forums.xilinx.com/t5/Embedded-Linux/Linux-driver-for-AXI-Quad-SPI-v3-2-in-Zynq/td-p/551595

    If you are using the PS SPI controller here:

    https://forums.xilinx.com/t5/Embedded-Linux/Issues-with-PS-SPI-in-linux/m-p/471400#M9430

    When you get this working, would you please share back with our community what your solution is?

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 10 years ago

    Hi Sana,

    Are you hooking up the PL AXI QSPI controller?  If so, take a look at this thread here:

    https://forums.xilinx.com/t5/Embedded-Linux/Linux-driver-for-AXI-Quad-SPI-v3-2-in-Zynq/td-p/551595

    If you are using the PS SPI controller here:

    https://forums.xilinx.com/t5/Embedded-Linux/Issues-with-PS-SPI-in-linux/m-p/471400#M9430

    When you get this working, would you please share back with our community what your solution is?

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • ashahsana
    0 ashahsana over 10 years ago in reply to zedhed

    Thanks for your Reply
    Actually i want to connect spi through EMIO
    My dts is
    ps7_spi_1: ps7_spi@e0006000 {
    tttcompatible = "xlnx,ps7_spi_1-4.03.a";
    tttreg = <0xe0006000 0x1000>;
    ttt#address-cells=<1>;
    ttt#size-cells=<0>;
    tttcurrent-speed = <115200>;t
    tttclock-frequency = <10000000>;t
    tttxlnx,data-bits = <8>;
    tttxlnx,odd-parity = <0>;
    tttxlnx,use-parity = <0>;
    tttspidev@0{
    ttttcompatible="spidev";
    ttttreg =<0>; //chipselect 0
    ttttspi-max-frequency= <50000000>;
    ttt};
    tt};

    I am using 7z020 board and because this is my first attempt to make device tree i used the information from
    https://github.com/torvalds/linux/blob/master/Documentation/devicetree/bindings/xilinx.txt
    and then i made devicetree.dtb after that when i boot the board i got the following error


    U-Boot 2013.01 (Apr 18 2013 - 10:02:30)

    DRAM:  512 MiB
    WARNING: Caches not enabled
    MMC:   zynq_sdhci: 0
    SF: Unsupported manufacturer 00
    *** Warning - spi_flash_probe() failed, using default environment

    In:    serial
    Out:   serial
    Err:   serial
    Net:   Gem.e000b000
    Hit any key to stop autoboot:  0
    Copying Linux from SD to RAM...
    Device: zynq_sdhci
    Manufacturer ID: 1b
    OEM: 534d
    Name: SMI
    Tran Speed: 50000000
    Rd Block Len: 512
    SD version 2.0
    High Capacity: Yes
    Capacity: 3.7 GiB
    Bus Width: 4-bit
    reading uImage
    2883472 bytes read in 391 ms (7 MiB/s)
    reading devicetree.dtb
    7166 bytes read in 15 ms (465.8 KiB/s)
    reading uramdisk.image.gz
    3780885 bytes read in 507 ms (7.1 MiB/s)
    ## Booting kernel from Legacy Image at 03000000 ...
       Image Name:   Linux-3.8.0-xilinx
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    2883408 Bytes = 2.7 MiB
       Load Address: 00008000
       Entry Point:  00008000
       Verifying Checksum ... OK
    ## Loading init Ramdisk from Legacy Image at 02000000 ...
       Image Name:
       Image Type:   ARM Linux RAMDisk Image (gzip compressed)
       Data Size:    3780821 Bytes = 3.6 MiB
       Load Address: 00000000
       Entry Point:  00000000
       Verifying Checksum ... OK
    ## Flattened Device Tree blob at 02a00000
       Booting using the fdt blob at 0x02a00000
       Loading Kernel Image ... OK
    OK
       Loading Ramdisk to 1f7ba000, end 1fb550d5 ... OK
       Loading Device Tree to 1f7b5000, end 1f7b9bfd ... OK

    Starting kernel ...


    Error: unrecognized/unsupported device tree compatible list:
    [ 'xlnx,zynq-7000' ]

    Available machine support:

    ID (hex)        NAME
    ffffffff        ARM-Versatile Express
    000008e0        ARM-Versatile Express
    00000d32        Xilinx Zynq Platform

    Please check your kernel config and/or bootloader.