Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design zedboard fmc
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 360 subscribers
  • Views 895 views
  • Users 0 members are here
Related

zedboard fmc

Former Member
Former Member over 11 years ago

hi
I am currently working on zedboard ZC702 along with ad-fmcomms1-ebz...My need is to transmit and receive signals using both the boards..My doubt is that how to assign pin configurations for fmc of zedboard???  what are the steps to be followed to transmit a digital data through fmc of zedboard to DAC present at ad-fmcomms1-ebz????help me plz to have a clear idea of assigning pins of fmc....

  • Sign in to reply
  • Cancel
Parents
  • narrucmot
    0 narrucmot over 11 years ago

    If you are looking to use the FMCOMMS1 FMC with the ZC702 or ZedBoard, you may want to look at the example designs and SD card images posted here:
    http://wiki.analog.com/resources/eval/user-guides/ad-fmcomms1-ebz/quickstart/zynq

    In general the XDC constraints for mapping the Zynq device pin to the FMC connector are something like this:
    set_property PACKAGE_PIN <pin_number> [get_ports {<port_name>}]

    You will also need to set the voltage standard:
    set_property IOSTANDARD LVCMOS<xx> [get_ports -filter { IOBANK == 35 } ]

    See this posted XDC file for a complete example:
    http://zedboard.org/sites/default/files/documentations/zedboard_master_XDC_RevC_D_v1a.zip

    To map the FMCOMMS1 FMC signals to the Zynq device correctly you will need the schematics for the FMC module (wiki.analog.com) and ZedBoard (http://zedboard.org/sites/default/files/documentations/ZedBoard_RevD.2_Schematic_130516.pdf).

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • narrucmot
    0 narrucmot over 11 years ago

    If you are looking to use the FMCOMMS1 FMC with the ZC702 or ZedBoard, you may want to look at the example designs and SD card images posted here:
    http://wiki.analog.com/resources/eval/user-guides/ad-fmcomms1-ebz/quickstart/zynq

    In general the XDC constraints for mapping the Zynq device pin to the FMC connector are something like this:
    set_property PACKAGE_PIN <pin_number> [get_ports {<port_name>}]

    You will also need to set the voltage standard:
    set_property IOSTANDARD LVCMOS<xx> [get_ports -filter { IOBANK == 35 } ]

    See this posted XDC file for a complete example:
    http://zedboard.org/sites/default/files/documentations/zedboard_master_XDC_RevC_D_v1a.zip

    To map the FMCOMMS1 FMC signals to the Zynq device correctly you will need the schematics for the FMC module (wiki.analog.com) and ZedBoard (http://zedboard.org/sites/default/files/documentations/ZedBoard_RevD.2_Schematic_130516.pdf).

    --Tom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data