Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design ZedBoard SD card extender
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 353 subscribers
  • Views 257 views
  • Users 0 members are here
Related

ZedBoard SD card extender

ejubenville
ejubenville over 10 years ago

I am trying to use an off-the-shelf cable that extends the SD card on a ZedBoard, but it doesn't work.  The extender cable is 15" long, and works on other devices to extend their SD cards slots, but when used on the ZedBoard the board refuses to boot.  Nothing is displayed on the console, and the blue LED indicating a completed FPGA load doesn't come on.

Does anyone know any reason why the ZedBoard SD card couldn't be extended, or anything special I would have to do to make it work?

  • Sign in to reply
  • Cancel
Parents
  • ejubenville
    0 ejubenville over 10 years ago

    Did some debugging on the signals on the SD card extender.  Poor signal quality was observed at extended end socket on IO CMD pin 2 although CLK pin 5 had good edge integrity.  The passive 8pF probe probably changed/degraded measurement a little, but nonetheless CMD line had significant edge ringing.

    Reduced the length of flex ribbon assembly (with alternating grounds) to about 7u201D and the signal integrity improved.  ZedBoard was able to read the SD card properly.

    Knowing that the extender worked on a laptop PC without a problem, the unique characteristics of the ZedBoard SD card slot must certainly be a factor. 

    The fix is not fully validated over time or with anything but class 4 SD card.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ejubenville
    0 ejubenville over 10 years ago

    Did some debugging on the signals on the SD card extender.  Poor signal quality was observed at extended end socket on IO CMD pin 2 although CLK pin 5 had good edge integrity.  The passive 8pF probe probably changed/degraded measurement a little, but nonetheless CMD line had significant edge ringing.

    Reduced the length of flex ribbon assembly (with alternating grounds) to about 7u201D and the signal integrity improved.  ZedBoard was able to read the SD card properly.

    Knowing that the extender worked on a laptop PC without a problem, the unique characteristics of the ZedBoard SD card slot must certainly be a factor. 

    The fix is not fully validated over time or with anything but class 4 SD card.