Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design xapp1078 for zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 360 subscribers
  • Views 389 views
  • Users 0 members are here
Related

xapp1078 for zedboard

e14 Contributor
e14 Contributor over 13 years ago

Hello!
   I'm using a Zedboard and running simple AMP based on Xilinx XAPP1078. After I copy the files to the SD card,I power on the board.The screen show "Uncompressing Linux... done, booting the kernel.
B ",and the progam stop.what's the problem?
Many thanks !

  • Sign in to reply
  • Cancel
  • danci
    0 danci over 9 years ago

    Just go through the following process to get it fixed

    subsystem Auto hardware setting->Advance bootable image storage setting and select sd-card for boot image ,kernel image and dtb image setting

    in the system-top.dts I add the following lines

    &spi0 {
    is-decoded-cs = <0>;
    num-cs = <3>;
    status = "okay";
    spidev@0x01 {
    compatible = "spidev2";
    spi-max-frequency = <20000000>;
    reg = <1>;
    };
    };
    &spi1 {
    is-decoded-cs = <0>;
    num-cs = <3>;
    status = "okay";
    spidev@0x00 {
    compatible = "spidev1";
    spi-max-frequency = <20000000>;
    reg = <1>;
    };
    };

    build the images

    $petalinux-build

    generate BOOT.BIN:

    $petalinux-package --boot --format BIN --fsbl ~/Avnet-Digilent-ZedBoard-2015.2/tutuapp.vipimages/linux/zynq_fsbl.elf --fpga ~my_program/my_program.sdk/system_wrapper_hw_platform_0/system_wrapper.bit --u-boot

    generate rootfs.cpio with the following command because I want to boot the board with sd-card

    $petalinux-package --image -c rootfs --format initramfs

    IN the sd card copy BOOT.BIN , image.ub and system.dtb into BOOT partition and rootfs.cpio into rootfs partition then run the following command

    $sudo pax -rvf rootfs.cpio

    In the last boot the board with this sd card

    and the result is, I cannot find any /dev/spidev

    even whatever changes I made in the sytem-top.dts after running the above commands these changes has been removed and the file name is system.dts, I also checked result is same if i am not adding the above defined lines in the system-top.dts