Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Use two pmod cameras on zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 721 views
  • Users 0 members are here
Related

Use two pmod cameras on zedboard

e14 Contributor
e14 Contributor over 10 years ago

I'm building stereoscopic applications on FPGA and using a zedboard as development board.
I want to use two cameras mt9d111 like this one:
http://www.aliexpress.com/store/product/Wang-MT9D111-camera-module/507962_539116520.html

I have a question regarding pmods, for this kind of sensor i need at least 12 pins for each camera, and there are just 20 GPIO available in the (non differential) pmods.

Is there a way to use at the same time a couple of these sensors?

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 10 years ago

    The differential Pmods can be used as single-ended as well without issue. Each 2x6 Pmod provides access to 8 I/Os. If you need 24 I/Os total, then you could have enough I/Os in 3 Pmods. There is no electrical issue using multiple Pmods simultaneously. You will need to build your IP in the design with proper timing and location constraints to see if your IP will fit and meet timing.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to bhfletcher

    i was not sure about the differential, this solves my doubt, thank you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Was you successful with implementing IP for this case?
    I'm also need such component and choose whether to do it myself or find something ready.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Was you successful with implementing IP for this case?
    I'm also need such component and choose whether to do it myself or find something ready.