Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Intefacing usb webcam on Zedboard running petalinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 360 subscribers
  • Views 2396 views
  • Users 0 members are here
Related

Intefacing usb webcam on Zedboard running petalinux

e14 Contributor
e14 Contributor over 10 years ago

Hi everyone.
I'm trying to build an application which involve usb webcam interfacing. Here're what I've done:
- Install petalinux and Avnet-Digilent-ZedBoard-2015.4 BSP from Xilinx
- Configure the kernel's device drivers to enable UVC by doing:
petalinux-config -c kernel
Device Drivers > Multimedia Support > Media USB Adapter > USB Video Class (UVC) (also UVC Input Event Support)
- Exclude USB 2.0 OTG FSM Implementation in Device Drivers > USB Support
- the other configurations are left by default
- Build the kernel by running
petalinux-build
- Pack the boot image by runnung
petalinux-package --boot --fsbl <path_to_fsbl_elf> --fpga <path_to_download.bit> --uboot

- Copy BOOT.bin in the root folder of Avner BSP and image.ub in ./images/linux to SD card
- set the jumper, boot up the board from SD card and connect webcam in the USB OTG port

"dmesg | tail" shows nothing related to webcam, so does "ls /dev" (no videox device listed),

What did I miss? Please response.... I can't find support anywhere.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    I finally got it to work by following this instruction:
    http://www.wiki.xilinx.com/Zynq+Linux+USB+Device+Driver
    to include neccessary driver and modify the device tree

    An important step is to short the jumpers on both sides of the otg port, to change the capacity of the port when working in host mode, and to supply power to connected usb devices.

    Rebuild the kernel, boot up the board, and a lovely message appears in the console right after a webcam is connect in the usb otg port.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to e14 Contributor

    Hello that is great.

    Which camera are you using? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to e14 Contributor

    Hello that is great.

    Which camera are you using?