Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design dongle Wifi 802.11n
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 360 subscribers
  • Views 850 views
  • Users 0 members are here
Related

dongle Wifi 802.11n

e14 Contributor
e14 Contributor over 11 years ago

Hello,

Can someone tell me if is it possible to connect a dongle wifi 802.11n to UART in Zedboard? Is it work? I need to connect to uart, because in the usb otg is the keyboard.

I am using the xillinux.

Thanks in advance for help.

Best regards

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hello,

    I suggest checking the log (i.e. "dmesg" on command problem or looking in /var/log/syslog) for what happens when the USB dongle is inserted.

    But odds are that a driver needs to be installed. Note that the driver can be compiled natively on the board's processor. That is, treat Zedboard as a regular computer. The kernel headers are installed in the distribution.

    Regards,
       Eli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Thanks in advance.

    When check the log the give a error: Firmware rtlwifi/rtl8192cufw.bin not available. (when the USB dongle connect).

    Do you know how can I fix?

    After that, in the top in icon of connection will show all wifi networks or do I need to do something to show the wifi available?

    Thanks very much for every help.

    best regards,
    Eduardo

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hello,

    The error kind-of speaks for itself. The driver exists and was loaded, but the firmware file was missing. Odds are that if you Google for the desired file name, you'll find a copy of it. If you put this file as /lib/firmware/rtlwifi/rtl8192cufw.bin in your system, there's a good chance that the Wifi icon will appear on the desktop.

    To make life easier for you: The "official" place for Linux firmware is this git repository:

    http://git.kernel.org/cgit/linux/kernel/git/firmware/linux-firmware.git

    The desired file can be found at

    http://git.kernel.org/cgit/linux/kernel/git/firmware/linux-firmware.git/plain/rtlwifi/rtl8192cufw.bin

    Regards,
       Eli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Thanks very much. That's error is now fixed.

    I am sorry, but I am very new in linux. As you can see in the picture: http://s15.postimg.org/y76u5rvju/20150712_140946.jpg


    The driver is install and the firmware are ok. But now there is nothing about wifi, how is it appear? How can I configure and show the wireless network to connect the board to internet?

    Thanks for all support.

    Best regards,
    Eduardo

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Thanks very much. That's error is now fixed.

    I am sorry, but I am very new in linux. As you can see in the picture: http://s15.postimg.org/y76u5rvju/20150712_140946.jpg


    The driver is install and the firmware are ok. But now there is nothing about wifi, how is it appear? How can I configure and show the wireless network to connect the board to internet?

    Thanks for all support.

    Best regards,
    Eduardo