Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design PLL Clock isn't working with FSBL
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 675 views
  • Users 0 members are here
Related

PLL Clock isn't working with FSBL

Former Member
Former Member over 10 years ago

Hi, I work with Xilinx Vivado tools.
I have a design with a custom AXI IP, which receives FCLK_CLK0. When I program the FPGA from the SDK, and run the SW I wrote, everything works great and the clock is running (I'm sensing it via a dedicated port).

On the other hand, if I create a boot image (using a basic FSBL I created with the SDK wizard), and starting up the Zedboard with an SD card, the clock isn't running. I'm guessing the FSBL didn't initiated it, but I can't find out how to solve it.

Needless to say, I asked old Google for a solution, but no avail.

Please help.

Thanks,
David.

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 10 years ago

    Make sure that you have added all of the partitions required for your design in the boot.bin you are generating. At a minimum it sounds like you will need your FSBL.elf, a bit file (system_wrapper.bit) and your application .elf file.

     

     

    There is a good example of how to do this in Tutorial 04 for the MicroZed board found here (same flow should work for the ZedBoard):

     

    http://zedboard.org/support/design/1519/10

     

    If you are still having issues you might try exporting your hardware design to SDK again and 'clean' and 'rebuild' your project.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago

    I did it exactly as the tutorial says, and still no clock.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago

    Well, the problem was solved by updating the Vivado software package... Thanks anyway!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer