Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design ZedboardOLED-v1.0-IP
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 333 views
  • Users 0 members are here
Related

ZedboardOLED-v1.0-IP

e14 Contributor
e14 Contributor over 11 years ago

An open source IP core for the Zedboard OLED was released today by Texas A&M University/Qatar.

The ZedboardOLED IP core provides a user friendly interface to the 128x32 organic LED display available on the Zedboard development board, a driver is supplied with the package, enabling a standalone usage for the display. The design can be easily modified to target other embedded platforms, provided with the package a step-by-step quick start up guide for using the IP.

Features 1 Plug and play using Vivado design suite. 2 Hierarchical open-source design, it can be easily altered to fit other systemsu2019 requirements. 3 Internal display buffer. 4 English characters bit maps are cached inside the controller. 5 Implemented driver for alphanumeric display .

This work was done as part of teaching materials for the ECEN 449 class offered at Texas A&M University/Qatar.

Written by Ali Aljaani/Texas A&M University at Qatar.

https://github.com/ama142/ZedboardOLED-v1.0-IP

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi,
    I am using Xilinx ISE 14.4. I want to use this IP core in my EDK design. How can I convert this vivado compatible IP to a EDK compatible IP? any help appreciated.

    Regards,
    Sandip

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi,
    I am using Xilinx ISE 14.4. I want to use this IP core in my EDK design. How can I convert this vivado compatible IP to a EDK compatible IP? any help appreciated.

    Regards,
    Sandip