Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Program FPGA from SDK and FMC
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 745 views
  • Users 0 members are here
Related

Program FPGA from SDK and FMC

Former Member
Former Member over 10 years ago

Hi,
I have a custom board that is connected to the FMC connector. The board itself houses a chip which gets signals from the FPGA. The board is passive.

When I connect the custom board to the Zedboard, and try to program the FPGA from the Xilinx SDK, I get an error that it can't connect to the zedboard:

ERRORt: FPGA Configuration failed.
Connection to Board Failed


    Unknown Error Occured
    Cable is not powered-on

If I disconnect the custom board and try to program the FPGA, it works.

Please help.

Thanks,
David.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 10 years ago

    The ZedBoard automatically adds the FMC to the JTAG chain when an FMC card is plugged into the board (via the FMC-PRSNT signal being pulled low/active). You can see details in the ZedBoard HW Users Guide and schematic that you can download here: http://picozed.org/support/documentation/1521
     
    You will need to add the FMC Card JTAG to your JTAG chain in Vivado for it to operate correctly or modify your FMC board to not assert FMC-PRSNT.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago

    The ZedBoard automatically adds the FMC to the JTAG chain when an FMC card is plugged into the board (via the FMC-PRSNT signal being pulled low/active). You can see details in the ZedBoard HW Users Guide and schematic that you can download here: http://picozed.org/support/documentation/1521
     
    You will need to add the FMC Card JTAG to your JTAG chain in Vivado for it to operate correctly or modify your FMC board to not assert FMC-PRSNT.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data