Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design RGMII at 3.3V
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 717 views
  • Users 0 members are here
Related

RGMII at 3.3V

e14 Contributor
e14 Contributor over 13 years ago

I see that the Zed board connects the Ethernet at 1.8V in bank 501. Is it possible to make this bank 3.3V and run the RGMII at this voltage? I've heard there may be an issue with Zynq-7000 running RGMII at 3.3V. It does appear that this may be the case since the Zed has the bank at 1.8V and has to use a voltage translator to get 3.3V at the SD interface instead of just changing the bank voltage to 3.3V.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I found a note in the documentation that confirmed my suspicion that the RGMII interface can't run at LVCMOS33.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I found a note in the documentation that confirmed my suspicion that the RGMII interface can't run at LVCMOS33.